Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84558members
353825posts

Change the solution proposed by the Ecodial for a variable motor load

EcoStruxure Power Design Forum

Collaborate with your peers on Electrical Network Design and Calculation Software(Ecodial, Electrical Calculation Tools) - ask questions and get answers from Schneider Electric experts and peers. Share your experience.

Solved
SergiyZolotarev
Ensign Ensign
Ensign
0 Likes
6
1307

Change the solution proposed by the Ecodial for a variable motor load

Hello
Is it possible to change the solution proposed by the Ecodial for a variable motor load with a soft starter (variable speed driver)?


Thanks, 

Sergiy
2021-04-01 134013.png

 


Accepted Solutions
Genghiz
Lt. Commander Lt. Commander
Lt. Commander
0
1268

Re: Change the solution proposed by the Ecodial for a variable motor load

Thanks for your comments and opinion; 

The point noted and transferred to the product development team.

This will go as part of the requirements list.

 

See Answer In Context

Tags (1)
6 Replies 6
Karthikeyan1
Ensign Ensign
Ensign
1
1304

Re: Change the solution proposed by the Ecodial for a variable motor load

Hello,

 

Thanks for your question. 

 

As of now, user cannot able to change the Motor starters manually. But EPD-Ecodial take care on the coordination between Circuit breaker and the Motor Starter and it will propose the best possible solution.

 

 

Tags (1)
SergiyZolotarev
Ensign Ensign
Ensign
0 Likes
0
1299

Re: Change the solution proposed by the Ecodial for a variable motor load

Thanks for the answer.
If possible, please include Ecodial as a proposal for future capabilities: add a segment and process selection function, conditions for applying motor load (for example, for a solution with the same power: fan - ATS22, conveyor - ATS48)
Thank you, Sergiy

Tags (1)
Genghiz
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
3
1297

Re: Change the solution proposed by the Ecodial for a variable motor load

Hello 

Thanks for your query about Ecodial.

 

From the given image; it's understood that you are looking for a 'different start up type' for the selected 'motor power'.

 

Suggestion:

Kindly please use the function "launch motor wizard" to find the available "start up types" for the selected motor powers. 

we can this explanation in the following images.launch motor wizardlaunch motor wizard

 

then make the selection accordingly.

 

Find_the start up type.png

 

Once after making all these selection of INPUTS, the "calculate project" will bring the "Solution."

 

Hope the above helps you to get your job done.

Tags (1)
SergiyZolotarev
Ensign Ensign
Ensign
0 Likes
2
1295

Re: Change the solution proposed by the Ecodial for a variable motor load

Hello
no, I was looking for a soft starter solution, but not for the fan, for the conveyor
Ecodial offered me ATS22, but based on the nature of the load, I understand that the best solution would be to use ATS48 (this is also confirmed by the EcoStruxure ™ Motor Control Configurator )

 

Tags (1)
SergiyZolotarev
Ensign Ensign
Ensign
0 Likes
1
1272

Re: Change the solution proposed by the Ecodial for a variable motor load

Hello
the proposal about which I speak is implemented (with the minimum possible options) for variable speed drivers, see figure.
I would like this opportunity to be available for soft starters as well.
Best regards, Sergiy

 

2021-04-02 104138.png

Tags (1)
Genghiz
Lt. Commander Lt. Commander
Lt. Commander
0
1269

Re: Change the solution proposed by the Ecodial for a variable motor load

Thanks for your comments and opinion; 

The point noted and transferred to the product development team.

This will go as part of the requirements list.

 

Tags (1)