Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84606members
353882posts

StruxureWareItOptimizeWithServerAccess-setup-7.5.2.windows.x64

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

DCIM_Support
Picard
Picard
0 Likes
2
160

StruxureWareItOptimizeWithServerAccess-setup-7.5.2.windows.x64

This question was originally posted on DCIM Support by Davis Navarro on 2019-06-19


I'm trying to install ito 7.5.2, but I'm getting the following error, some idea


 

(CID:145425569)

2 Replies 2
DCIM_Support
Picard
Picard
0 Likes
0
160

Re: StruxureWareItOptimizeWithServerAccess-setup-7.5.2.windows.x64

This answer was originally posted on DCIM Support by Greg Sterling on 2019-06-20


When you attempted to install ITO did you specify an alternate installation directory/folder? There was a bug in this ITO release which would yield that error if a non-standard installation path was used.

If yes, the current ITO release, 7.5.6 has a fix for that issue. That download is on the same download page as current DCO releases.

Regards

Greg Sterling

(CID:145850488)

DCIM_Support
Picard
Picard
0 Likes
0
160

🔒 Closed

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.