Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84571members
353844posts

Powerchute integration with DCE

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Solved
DCIM_Support
Picard
Picard
0 Likes
9
485

Powerchute integration with DCE

This question was originally posted on DCIM Support by Vineet K. Sarin on 2016-03-01


Hi,

I would like to check whether we can integrate Powerchute Business Edition with Struxureware DCE. The idea is to bring UPS from 1 to 3 kva also under DCE Monitoring domain. I have heard that Powerchute has snmp v1/v2/v3 OUT CAPABILITIES and also offers MIB file.  I feel in that case we can easily integrate the same into DCE using a custom DDF?

Anyone who has tried that before or any snapshots will be appreciated!

 

(CID:105467272)


Accepted Solutions
DCIM_Support
Picard
Picard
0 Likes
0
485

Re: Powerchute integration with DCE

This answer was originally posted on DCIM Support by Michael Chrustowicz on 2016-03-01


Hello Vineet

PowerChute Business Edition Agent for Windows can pass information to  Windows SNMP Service.

This will allow you to monitor these Agents (UPS-s) in DCE - you do not need any DDF for this, it is already included in DCE. You need to make sure Windows SNMP Service is setup correctly see following link:

http://www.apc.com/site/support/us/en/faq/?page=content&country=ITB&lang=en&locale=en_US&id=FA159596...

 

Regards

Michael

 

(CID:105467357)

See Answer In Context

9 Replies 9
DCIM_Support
Picard
Picard
0 Likes
4
485

Re: Powerchute integration with DCE

This answer was originally posted on DCIM Support by Christopherus Laurentius on 2016-03-01


Hi Vineet,

Had the same ideas before, exactly on what you are trying to attempt.

It was not realized though, so I can't comment on the outcome.

Personally, I prefer via NMC.

 

Regards,

Chris

(CID:105467295)

DCIM_Support
Picard
Picard
0 Likes
0
484

Re: Powerchute integration with DCE

This comment was originally posted on DCIM Support by Christopherus Laurentius on 2016-03-01


I'll email you my test with PCBE and drawing separately.

(CID:105467298)

DCIM_Support
Picard
Picard
0 Likes
0
484

Re: Powerchute integration with DCE

This comment was originally posted on DCIM Support by Vineet K. Sarin on 2016-03-01


Can I get it today itself as it is urgent for a Tender and will decide whether we should go ahead with this architecture or not... Also when it comes to 1 KVA ranging till 6 KVA do all of them have the same NMC cards which can be pulled directly over DCE? If not then how will we pull these UPS on DCE we have to go through Powerchute channel , what do you say?

(CID:105467299)

DCIM_Support
Picard
Picard
0 Likes
0
484

Re: Powerchute integration with DCE

This comment was originally posted on DCIM Support by Christopherus Laurentius on 2016-03-01


Check your email? I just sent after posting 🙂 From what I know, any UPS 5KVA onwards has NMC, but I heard newer models like SURTA comes with NMC built in, so do check your UPS model & NMC locally. Regards, Chris

(CID:105467300)

DCIM_Support
Picard
Picard
0 Likes
0
484

Re: Powerchute integration with DCE

This comment was originally posted on DCIM Support by Steven Marchetti on 2016-03-01


Hi guys, Just an FYI, there is no problem adding a PCBE agent to DCE. You need to configure SNMP first, then install the agent, then monitor with DCE. One major caveat however is that there are no essential alerts. This means there are no pre-configured thresholds and you must manually create any threshold such as on-battery or bad battery. Steve

(CID:105467361)

DCIM_Support
Picard
Picard
0 Likes
0
486

Re: Powerchute integration with DCE

This answer was originally posted on DCIM Support by Michael Chrustowicz on 2016-03-01


Hello Vineet

PowerChute Business Edition Agent for Windows can pass information to  Windows SNMP Service.

This will allow you to monitor these Agents (UPS-s) in DCE - you do not need any DDF for this, it is already included in DCE. You need to make sure Windows SNMP Service is setup correctly see following link:

http://www.apc.com/site/support/us/en/faq/?page=content&country=ITB&lang=en&locale=en_US&id=FA159596...

 

Regards

Michael

 

(CID:105467357)

DCIM_Support
Picard
Picard
0 Likes
1
484

Re: Powerchute integration with DCE

This answer was originally posted on DCIM Support by Yoshinobu Suzuki on 2016-03-09


Hi Vineet,

I shared the idea, because of the broad user base of PCBE here.

I attached some screen shots what sensors can be collected by DCE7.2.7 from PCBE v9.1.1 on Windows 2012R2 with Smart UPS 1200.

best regards,

Yoshi

(CID:105468147)

DCIM_Support
Picard
Picard
0 Likes
0
484

Re: Powerchute integration with DCE

This comment was originally posted on DCIM Support by Yoshinobu Suzuki on 2016-03-09


You can change "Device Type" in DCE from "Server/Workstation" to "UPS" if you want, but you cannot change "Model." It will be collected from the local Server OID. Serial Number seems to be the serial of Smart UPS 1200.

(CID:105468157)

DCIM_Support
Picard
Picard
0 Likes
0
484

🔒 Closed

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.