Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84849members
354307posts

Netbotz 450/500 FOR Telecom remote shelter monitoring

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

DCIM_Support
Picard
Picard
0 Likes
5
426

Netbotz 450/500 FOR Telecom remote shelter monitoring

This question was originally posted on DCIM Support by Vineet K. Sarin on 2014-06-13


Hi, I don't have a usual Internet connection for the Netbotz to be accessed and so I need a device like Netbotz which can be hooked with 3g Modem or a data card through which it can get Internet connectivity and we can pull all these on a common web interface.

Does Netbotz have such a facility?

(CID:84115459)

5 Replies 5
DCIM_Support
Picard
Picard
0 Likes
0
426

Re: Netbotz 450/500 FOR Telecom remote shelter monitoring

This comment was originally posted on DCIM Support by Søren Bruncke Mikkelsen on 2014-06-16


To my understanding the Netbotz devices will be able to send alarms, notifications etc. using a modem. I do not think there can be any build in card to give access to the common web interface. I guess that would have to be a "stand alone" setup where the Netbotz device then can be connected using its wired network interface.

(CID:84836353)

DCIM_Support
Picard
Picard
0 Likes
0
426

Re: Netbotz 450/500 FOR Telecom remote shelter monitoring

This answer was originally posted on DCIM Support by rtoole on 2014-06-16


Hi Vineet,

 

NetBotz 400 and 500 appliances have USB ports.  We support a few USB modems which are capable of sending SMS and email alerts.  Is there functionality beyond this the customer is looking for?

 

Ryan

(CID:84836390)

DCIM_Support
Picard
Picard
0 Likes
0
426

Re: Netbotz 450/500 FOR Telecom remote shelter monitoring

This answer was originally posted on DCIM Support by Vineet K. Sarin on 2014-06-17


Do you have a list of Modems that are supported for India?

(CID:84836396)

DCIM_Support
Picard
Picard
0 Likes
0
426

Re: Netbotz 450/500 FOR Telecom remote shelter monitoring

This answer was originally posted on DCIM Support by Søren Bruncke Mikkelsen on 2014-06-17


A list of supported modems can be seen here: http://dcimcommunity.com/questions/83656794/which-modem-is-supported-by-netbotz-v3

 

/Søren

(CID:84836400)

DCIM_Support
Picard
Picard
0 Likes
0
426

🔒 Closed

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.