Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84297members
353446posts

Floor tile airflows did not add up to downflow CRAC airflows

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Solved
DCIM_Support
Picard
Picard
0 Likes
8
691

Floor tile airflows did not add up to downflow CRAC airflows

This question was originally posted on DCIM Support by Gleb Tyunikov on 2018-08-30


Hello guys,

I ran into a bit of a problem..
First of all in my Data Center i have few hot aisle containment pods, and we have inrow's for cooling.

After the placement of the racks and the inrows in a closed aisle I can see in the cooling tab that all racks are green - they all getting enough cooling.
I have yet to install my temperature sensor so i want to see the calculated map in the 3D veiw model.
When i try to see it, it throws me this message "Floor tile airflows did not add up to downflow CRAC airflows


I've read in other threads that this happens when you use non apc inrow, and so I changed it and placed an apc ones instead and still, i get this Error message..

Could you please help me to find the solution to this?

Thank you,
Gleb Tyunikov

(CID:134024383)

Tags (1)

Accepted Solutions
DCIM_Support
Picard
Picard
0 Likes
4
691

Re: Floor tile airflows did not add up to downflow CRAC airflows

This answer was originally posted on DCIM Support by Jef Faridi on 2018-08-30


Hi Gleb,

As illustrated in the following image, I have used one "InRow RC 300mm Standard" unit without any problem:

I think to understand your issue, I would need more details about the setup - can you provide a copy of your backup file (shared safely with me)?

Kind regards

(CID:134024443)

See Answer In Context

8 Replies 8
DCIM_Support
Picard
Picard
0 Likes
0
691

Re: Floor tile airflows did not add up to downflow CRAC airflows

This comment was originally posted on DCIM Support by Jef Faridi on 2018-08-30


Hi Gleb,

Can you please share screen captures illustrating which cooling units/part numbers (from Genome Library) you are using, thanks.

Kind regards

(CID:134024422)

DCIM_Support
Picard
Picard
0 Likes
0
689

Re: Floor tile airflows did not add up to downflow CRAC airflows

This comment was originally posted on DCIM Support by Gleb Tyunikov on 2018-08-30


Hi jeff,

Unfortunately i cant share  a screenshot
But I'm using the APC 300mm standard units

Thank you

(CID:134024428)

DCIM_Support
Picard
Picard
0 Likes
4
692

Re: Floor tile airflows did not add up to downflow CRAC airflows

This answer was originally posted on DCIM Support by Jef Faridi on 2018-08-30


Hi Gleb,

As illustrated in the following image, I have used one "InRow RC 300mm Standard" unit without any problem:

I think to understand your issue, I would need more details about the setup - can you provide a copy of your backup file (shared safely with me)?

Kind regards

(CID:134024443)

DCIM_Support
Picard
Picard
0 Likes
0
689

Re: Floor tile airflows did not add up to downflow CRAC airflows

This comment was originally posted on DCIM Support by Gleb Tyunikov on 2018-08-30


Well as i said earlier its not possible to share any screenshots or backup files..

But I will be more than happy to provide you with specific technical information...

What is strange to me in my situation is that in the cooling tab i can see that the racks are getting cooled and are using right temperatures and only the 3D representation wouldn't work..

When the InRow is placed, is there any specific information that has to stay written on it? like in your picture the "manufacturer" "model" any else?  

(CID:134024456)

DCIM_Support
Picard
Picard
0 Likes
0
689

Re: Floor tile airflows did not add up to downflow CRAC airflows

This comment was originally posted on DCIM Support by Jef Faridi on 2018-08-30


Hi Gleb,

I was able to reproduce:

As illustrated, if I customize a copy of my InRow cooling unit (by replacing APC with another manufacture) in my Genomes. And then drag this to the floor and run 3D temp calculations, then I see a similar notification as you've mentioned:

I will capture a bug report for this.

 

Workaround:

If I use the InRow cooling unit (without modification) and drag it to the floor:

And then change the manufacture name for this unit on the floor:

Now I can run the 3D temperate simulation without any problem:

Kind regards

(CID:134024488)

DCIM_Support
Picard
Picard
0 Likes
0
689

Re: Floor tile airflows did not add up to downflow CRAC airflows

This comment was originally posted on DCIM Support by Gleb Tyunikov on 2018-08-30


Amazing,

Thank you very much Jeff

have a great day!

(CID:134024496)

DCIM_Support
Picard
Picard
0 Likes
0
689

Re: Floor tile airflows did not add up to downflow CRAC airflows

This comment was originally posted on DCIM Support by Jef Faridi on 2018-08-30


You are most welcome, Gleb

have a great day, too

thanks.

Kind regards

(CID:134024499)

DCIM_Support
Picard
Picard
0 Likes
0
689

🔒 Closed

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.