Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84292members
353422posts

Empty unit space

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Solved
DCIM_Support
Picard
Picard
0 Likes
10
715

Empty unit space

This question was originally posted on DCIM Support by Andrius Gataveckas on 2019-05-07


Is it possible to allocate an empty unit space to a customer? If not, are there any plans to introduce a unit level management functionality?

(CID:143755952)


Accepted Solutions
DCIM_Support
Picard
Picard
0 Likes
8
715

Re: Empty unit space

This answer was originally posted on DCIM Support by Jef Faridi on 2019-05-07


Hi Andrius,

With DCO Colo it is possible to create an empty cage and allocate it to a customer.

Kind regards

(CID:143755975)

See Answer In Context

10 Replies 10
DCIM_Support
Picard
Picard
0 Likes
8
716

Re: Empty unit space

This answer was originally posted on DCIM Support by Jef Faridi on 2019-05-07


Hi Andrius,

With DCO Colo it is possible to create an empty cage and allocate it to a customer.

Kind regards

(CID:143755975)

DCIM_Support
Picard
Picard
0 Likes
0
715

Re: Empty unit space

This comment was originally posted on DCIM Support by Andrius Gataveckas on 2019-05-07


What if I have a rack that has 21 out of 42 units assigned for one customer, but the rest of 21 units are sold to another customer, who has not got anything installed. Is there a way to mark those units as allocated for that customer but not actually occupied?

(CID:143755988)

DCIM_Support
Picard
Picard
0 Likes
0
715

Re: Empty unit space

This comment was originally posted on DCIM Support by Ed Tarento on 2019-05-07


Hi Andrius

Do you have DCO Change?  You can reserve this and sync into your change management process.  Another simple solution is to create a 1U Genomes entry (I've used blanking panel as a template) and place the units in the U position for the client.  If you have DCO Capacity, you can tag the items, otherwise you can create a custom property or just name the items

Cheers

Ed

(CID:143756054)

DCIM_Support
Picard
Picard
0 Likes
0
715

Re: Empty unit space

This comment was originally posted on DCIM Support by Andrius Gataveckas on 2019-05-08


Hi Ed, no, we are not using DCO Change. If we create 1U genomes entries with blanking panels, will it then show that those units are occupied within the free space report? Thank you.

(CID:143756169)

DCIM_Support
Picard
Picard
0 Likes
0
715

Re: Empty unit space

This comment was originally posted on DCIM Support by Ed Tarento on 2019-05-08


Good point.  They will appear as occupied in the free space report. 

Another way of looking at it ...... Are these "reserved" U positions really "free"?  Can they be sold to another customer?    Perhaps "free" could mean empty and not reserved?  

Ed

(CID:143756191)

DCIM_Support
Picard
Picard
0 Likes
0
715

Re: Empty unit space

This comment was originally posted on DCIM Support by Andrius Gataveckas on 2019-05-08


Yes, "free" should mean empty. They cannot be sold to another customer.

(CID:143756217)

DCIM_Support
Picard
Picard
0 Likes
0
715

Re: Empty unit space

This comment was originally posted on DCIM Support by Jef Faridi on 2019-05-08


Hi Andrius,

In DCO, in general access rights/permission can be location, room, cage and/rack based. 

In your scenario, where one rack may be assigned to two different customers, then I can think of the following work-around:

a) if the DCO is not intended to be used/accessed by customers, then those free/"empty"/reserved U positions could be field (occupied) by non-powered devices, such as patch-panels. In this way assets(patch-panels) Tags and/or properties settings could be used to mark it for a certain customer... and would also appear in the reports.

b) if the DCO is intended to be used/access by customers, then "dividing" the 42 U rack to two smaller racks, eg. using two 21 U racks instead, could be considered. Downside: increase in used license, and also racks cannot be mounted on top of each other.

Kind regards

 

(CID:143756296)

DCIM_Support
Picard
Picard
0 Likes
0
715

Re: Empty unit space

This comment was originally posted on DCIM Support by Andrius Gataveckas on 2019-05-08


Hi Jef,

Thank you for your input, appreciate the answers. I guess we will have to select one of two workarounds, even though neither of them really suits the business requirement.

By any chance, do you happen to know if there are plans for future software releases to allow management on the unit level? Maybe it is possible to request it as a feature?

(CID:143756302)

DCIM_Support
Picard
Picard
0 Likes
0
715

Re: Empty unit space

This comment was originally posted on DCIM Support by Jef Faridi on 2019-05-08


Hi Andrius,

As far as I know U based access level never been discussed, but I will take your feed back to our management team, thanks.

Kind regards

(CID:143756309)

DCIM_Support
Picard
Picard
0 Likes
0
715

🔒 Closed

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.