Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84521members
353757posts

EBO (ES / AS) -> EBO integration via EWS

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

sesa241642
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
4
480

EBO (ES / AS) -> EBO integration via EWS

Hi there!

 

Is there a way of Adding EBO (Automation Server OR Enterprise Server) to Data Center Expert via EWS ?

 

We have already tested the below scenarios:

 

1. Adding DCE to EBO via EWS

2. Adding AS to DCE via DDFs

 

Would like to explore adding EBO to DCE via EWS, with no OR minimum DDF effort.

 

Thanks

AD

Tags (1)
4 Replies 4
masolans
Ensign
Ensign
0 Likes
3
474

Re: EBO (ES / AS) -> EBO integration via EWS

EBO can publish modbus register by tcp/IP and DCE can read it by a DDF or modbus module

Tags (1)
sesa241642
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
2
472

Re: EBO (ES / AS) -> EBO integration via EWS

@masolans , yes, this is what we have been doing.

 

The ask is more about EWS. Can DCE read EBO via EWS?

 

We are looking for a more scalable solution. When you add a DDF to read EBO, and if you have any alterations of devices at BMS end, you DDF is no longer valid.

 

We are looking for a seamless integration via EWS.

Tags (1)
tjlaw
Lieutenant Lieutenant
Lieutenant
0 Likes
0
468

Re: EBO (ES / AS) -> EBO integration via EWS

HI, 

 

 

DCE only supports Modbus TCP, SNMP (v1 &v3), and Netbotz appliance. DCE consume data from EBO via EWS is not supported. But EBO is able to consume data from DCE via EWS. 

 

Hope this helps. 

 

BR, 

 

TJ

Tags (1)
ATrabert
Lieutenant Lieutenant
Lieutenant
0 Likes
0
454

Re: EBO (ES / AS) -> EBO integration via EWS

As others have mentinoned, you cannot integrate EBO and DCE with EWS.  One solution to EBO presenting all devices as a single modbus device is to use a device like an SMC Field Server to break up a single modbus devices into multiple modbus devices, (eg 1 modbus address per device) and then discover them in DCE as separate devices with 1 ddf per unique device type.

 

This is a common ACS solution for integrating EBO and other 3rd party BMS' into DCE.  Then if you need to modify the BMS, as long as the other devices remain unchanged, you only need to have the field server programming modified and can add or remove devices to DCE.  If you add devices, you will also need new DDFs created.