Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84505members
353724posts

DCE MAC ADDRESS CHANGE

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

silvio.filho
Ensign
Ensign
0 Likes
1
333

DCE MAC ADDRESS CHANGE

Hello people!

 

Could anyone help me?

 

I Need to change the mac address from a DCE server, but when i start the server i receive the message below

 

DATA CENTER EXPERT IS UNABLE TO START DUE TO A MAC ADDRESS CHANGE

 

 

Tags (1)
1 Reply 1
Shaun
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
309

Re: DCE MAC ADDRESS CHANGE

Hi Silvio,

 

The only supported method to change the MAC address is to backup the server, deploy a new, and restore the backup to the new VM.

 

Because the MAC address is used to generate many internal identifiers, this process is required so that the data is migrated properly forcing new identifiers to be created.

Tags (1)