Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354358posts

ACRD301s sensors not shown in ITA

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

jzurera
Lieutenant
Lieutenant
0 Likes
1
328

ACRD301s sensors not shown in ITA

Hi team,

 

we have a deploy with ITA 9.3.0 and DCE 7.9.0 with inrow cooling units model ACRD301S. We are using DDFs ACRD2G v14 and ACRC301 v16. In DCE we see properly all the sensors but in ITA we do not see any sensor from these devices.

 

We have another issue in DCE, we receive the alarm "Device status may be inaccurate because an attempt to transfer a device definition file (DDF) failed"  in these inrows. We have the FTP server available in the inrows and also in DCE the Device File Transfer Settings configured for these inrows with their user/pass. 

 

Thanks in advance.

 

 

Tags (1)
1 Reply 1
Jef
Captain Captain
Captain
0 Likes
0
313

Re: ACRD301s sensors not shown in ITA

Hi Javier,

 

Concerning the problem in ITA, eg. device (ACRD301S) sensor data not be displayed, this could be a DDF related issue as ITA gets the device sensor data from the integrated system (DCE). You might want to contact the device support team for new DDF file, it can be requested via the webform here: https://helpcenter.ecostruxureit.com/hc/en-us/requests/new?ticket_form_id=360000111657

 

Kind regards,

Jef

Tags (1)