Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-04 09:11 PM . Last Modified: β2024-04-04 03:51 AM
how to set up alarms for UPS that is has 30% remaining life
(CID:132671933)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-04 09:11 PM . Last Modified: β2024-04-04 03:51 AM
Hi Muro,
If you want to create a manual threshold in DCE for 30% UPS battery, the first thing I suggest is looking at K-base FA299560 which can help walk you through creating thresholds in general.
To create a battery threshold, create an "Other Numeric Threshold", choose a minimum value, and look for battery capacity remaining.

Then you simply have to set that value to 30:

You may also want to consider something like battery time remaining for a threshold instead of (or in addition to) battery capacity. As batteries get older, they can't hold the load up for the same time they could when they were new. An older battery still charges to the full voltage and will show 100% capacity but it could be the difference between taking 20 minutes to exhaust the batteries with new batteries or it could be 2 minutes to exhaustion with old batteries. If the latter is the case, 30% battery capacity will only be 40 seconds...just something to consider.
This is all assuming an APC UPS. I can't say that all UPS (especially 3rd party units) have the same sensors. If there is no sensor for battery capacity remaining, you may have to consider other alternatives.
Steve
(CID:132671947)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-04 09:11 PM . Last Modified: β2024-04-04 03:51 AM
I presume you were referring to run time as well, but your phrasing made me wonder if you might actually be thinking about lifecycle management.
if so - the only thing I can think of would be around battery age - which is not consistently available to modify, and so not reliable, but if your UPS allows battery age or install date to be modified, you could monitor it and set an expiration or duration, in a manner similar to what was described.
(CID:133367624)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-04 09:11 PM . Last Modified: β2023-10-22 09:36 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Youβve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.