Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

NetBotz 750 with multiple sensor pod and DCE

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • NetBotz 750 with multiple sensor pod and DCE
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Cory_McDonald Champion
159
Jef
Jef Leader
114
gsterling
gsterling Mentor
77
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
Back to EcoStruxure IT Forum
Start a Topic
GaborNovak
GaborNovak
Contributor

Posted: ‎2020-10-12 12:32 AM

0 Likes
1
2215
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
Posted: ‎2020-10-12 12:32 AM

NetBotz 750 with multiple sensor pod and DCE

I have installed NetBotz 750 and 10 sensor pod. When I have imported the NetBotz 750 in the DCE I see just the NetBotz 750 device. I can’t see the sensor pods. It seems that the NetBotz 750 shows in the DCE that it’s just one device with multiple input.

When I have used NetBotz 250, 570, etc. The I can see the sensor pods and I can place them in different location.

I have renamed all sensor pods but this name doesn’t shows up in the DCE. For example I have two colocation in a data center, the two room has separated fire system. The fire system is integrated via dry contact cable in to the NetBotz 750.

You can see that the DCE shows just the dry contact name. In my case the two fire alarm (tuzjelzes) is in different location, but I can’t separate them.

 

NetBotz 750 fire system dry contact.png

 

How can I setup the NetBotz 750 to show the sensor pods?

How can I set the DCE to show the sensor pods which are connected to the system. I would like to place the pods in different rooms. Now all alarms is showed up  in the same location because the I can place the NetBotz 750 in one place.

Labels
  • Labels:
  • Data Center Expert
  • NetBotz
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Cory_McDonald
Cory_McDonald Champion
Champion

Posted: ‎2020-10-19 05:36 AM . Last Modified: ‎2020-10-19 05:37 AM

1 Like
0
2170
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
Posted: ‎2020-10-19 05:36 AM . Last Modified: ‎2020-10-19 05:37 AM

Hello @GaborNovak,

 

You can search for a newer 750 DDF here to try: https://ddf.ecostruxureit.com/

 

If there isn't a newer DDF than what you already have installed, you can click in the lower right to submit at ticket to the DDF team so that they can look into your request.

 

Kind Regards,

Cory

  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.