Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

DCO 8.3.2 - Vulnerability Report support

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • Re: DCO 8.3.2 - Vulnerability Report support
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Cory_McDonald Champion
160
Jef
Jef Leader
114
gsterling
gsterling Mentor
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
Back to EcoStruxure IT Forum
Start a Topic
Solved
Venkat
Venkat Explorer
Explorer

Posted: ‎2020-07-15 06:42 AM

0 Likes
1
2277
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
Posted: ‎2020-07-15 06:42 AM

DCO 8.3.2 - Vulnerability Report support

Hi team,

 

One of our customer, we have installed DCO 8.3.2 on Redhat Linux Enterprise -v7.6 Server. (Physical Server)

 

The customer sent the DCO Server Vulnerability Report and asking us to provide solution to fix the Vulnerability issues.

 

The Vulnerability Report is having 110 issues in various levels ( Critical, High, Medium, Low) .

 

Request you to verify the Report and Suggest us to provide the solution to the customer end.

 

Thanks & Regards,

 

K.Venkat.

Attachments
MUS-n-sk1121 - 1-07-2020.xlsx
Labels
  • Labels:
  • Data Center Operation
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
gsterling
gsterling Mentor
Mentor

Posted: ‎2020-07-15 07:18 AM

1 Like
0
2273
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
Posted: ‎2020-07-15 07:18 AM

Hello Venkat.

 

I'm pasting the same response as added to zendesk ticket # 74662

 

This is a new installation? When customers install DCO on Redhat they remain owners of the OS which means follow-up with redhat in this case may be required as its something we cannot control.

 

I assume the customer has an active subscription with redhat? If yes, they should plan to run a "yum update" to update the OS based modules. I suspect if they are older versions a number of the vulnerabilities will then be resolved assuming redhat has addressed them.

Regards

 

Greg Sterling

See Answer In Context

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
gsterling
gsterling Mentor
Mentor

Posted: ‎2020-07-15 07:18 AM

1 Like
0
2274
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
Posted: ‎2020-07-15 07:18 AM

Hello Venkat.

 

I'm pasting the same response as added to zendesk ticket # 74662

 

This is a new installation? When customers install DCO on Redhat they remain owners of the OS which means follow-up with redhat in this case may be required as its something we cannot control.

 

I assume the customer has an active subscription with redhat? If yes, they should plan to run a "yum update" to update the OS based modules. I suspect if they are older versions a number of the vulnerabilities will then be resolved assuming redhat has addressed them.

Regards

 

Greg Sterling
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.