Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Connecting multiple Camera Pod 165's to a NetBotz Wall Monitor 755

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • Re: Connecting multiple Camera Pod 165's to a NetBotz Wall Monitor 755
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Back to EcoStruxure IT Forum
Start a Topic
Solved
maayre
maayre
Contributor

Posted: ‎2025-09-10 11:58 AM

0 Likes
3
1662
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
Posted: ‎2025-09-10 11:58 AM

Connecting multiple Camera Pod 165's to a NetBotz Wall Monitor 755

According to the NetBotz 5.x User Guide, you can use a network switch or hub to connect up to four cameras - presumably including Camera Pod 165's to a NetBotz Wall Monitor 755 via the Private LAN port.

 

Can anybody recommend a manufacturer, model they have used to complete the above successfully.

 

Thanks in advance.

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
maayre
maayre
Contributor

Posted: ‎2025-11-20 09:42 AM

In response to maayre
0 Likes
0
1235
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
Posted: ‎2025-11-20 09:42 AM

All,

Related to this topic:

 

Following testing, I can confirm that it is possible to connect two Camera Pod 165's to a single NetBotz Wall Monitor 755 by means of connecting them to the Netgear GS305P 5-Port Gigabit PoE+ Compliant Unmanaged Network Switch and then connecting this to the Private LAN port.

 

Initially, one of the two Camera Pod 165's was reported as Not Authorized under the Devices screen, but after deleting the device and then rebooting the NetBotz Wall Monitor 755 it was then accessible.

 

NOTE: The Netgear GS305P 5-Port Gigabit PoE+ Compliant Unmanaged Network Switch has a PoE budget up to 63W Total so two Camera Pod 165's as required in this instance is possible, however, there is a model that supports up to 90W total so could potentially support three.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 3
JLehr
JLehr Champion
Champion

Posted: ‎2025-09-22 12:11 PM

1 Like
2
1624
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
Posted: ‎2025-09-22 12:11 PM

Hi @maayre 

To be clear, the user guide states:

 

You can connect a network switch or hub to the Private LAN ports to connect up to ten downstream devices, including up to four cameras. Performance may vary depending on the amount of video recorded or the number of sensors attached to your downstream devices.

 

Cameras refers to the NetBotz Camera Pod 165.

 

Please note that successful deployment will vary depending on factors other than hub/switch hardware.

 

Reply

Link copied. Please paste this link to share this article on your social media post.

maayre
maayre
Contributor

Posted: ‎2025-09-22 01:56 PM

In response to JLehr
0 Likes
1
1596
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
Posted: ‎2025-09-22 01:56 PM

Thanks for your reply @JLehr.

 

A couple of related updates for your and the wider groups awareness:

 

  1. Having separately consulted the EcoStruxure IT Data Center Expert Technical Support team - who also support NetBotz devices, they stated that Schneider Electric do not have a recommended manufacturer or model network switch or hub to be used in such instances.
  2. Having also consulted a member of our Network Services team, they suggested the Netgear GS305P 5-Port Gigabit PoE+ Compliant Unmanaged Network Switch as a possible option.

Does anybody in the community have experience either with the suggested switch or with a multi Camera Pod 165 set-up to a single NetBotz Wall Monitor 755? Please advise.

Reply

Link copied. Please paste this link to share this article on your social media post.

maayre
maayre
Contributor

Posted: ‎2025-11-20 09:42 AM

In response to maayre
0 Likes
0
1236
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
Posted: ‎2025-11-20 09:42 AM

All,

Related to this topic:

 

Following testing, I can confirm that it is possible to connect two Camera Pod 165's to a single NetBotz Wall Monitor 755 by means of connecting them to the Netgear GS305P 5-Port Gigabit PoE+ Compliant Unmanaged Network Switch and then connecting this to the Private LAN port.

 

Initially, one of the two Camera Pod 165's was reported as Not Authorized under the Devices screen, but after deleting the device and then rebooting the NetBotz Wall Monitor 755 it was then accessible.

 

NOTE: The Netgear GS305P 5-Port Gigabit PoE+ Compliant Unmanaged Network Switch has a PoE budget up to 63W Total so two Camera Pod 165's as required in this instance is possible, however, there is a model that supports up to 90W total so could potentially support three.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.