Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 12:57 AM . Last Modified: 2024-04-05 04:19 AM
On the https://dcimassets.schneider-electric.com site.
It does not seem to record the 25n license that comes with DCE and it would be nice if it could. If you look at any asset on the list then it will show any licenses that have been added since deployment, but not those that were included with the DC server appliance.
Is there a way to add a license key to an existing DCE appliance without going through 'Redeem Passcode'. I can't figure it out if there is.
Would be good for record keeping purposes...
Regards
(CID:126166619)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 12:57 AM . Last Modified: 2024-04-05 04:19 AM
Hi Garry,
No, there is no way to add it. If they started to add it, I believe it would sku the system especially when tech support verifies support contracts, they may not know if it was a 25 node or the default 25. Also customers unfamiliar with the change could be confused. Since you don't actually add the 25 node, I'm not sure it's necessary.
You can always put an enhancement request in the system but I doubt this will ever become part of the 7.x DCE systems. The next generation of "EcoStruxure" will be set up differently so something like this may work better with that software.
Steve
(CID:126166711)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 12:57 AM . Last Modified: 2024-04-05 04:19 AM
The license keys are also not showing within DCIM Assets because they are non-transferrable licensing. Only additional licensing is shown as the base server when you register it is known to have the 2 built-in licenses.
(CID:126166759)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 12:57 AM . Last Modified: 2023-10-20 05:05 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.