Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84429members
353627posts

Seconds counter

EcoStruxure Geo SCADA Expert Forum

Find out how SCADA systems and networks, like EcoStruxure Geo SCADA Expert, help industrial organizations maintaining efficiency, processing data for smarter decision making with IoT, RTU and PLC devices.

Solved
Valentino
Ensign Ensign
Ensign

Seconds counter

Good morning


I would need to count the hours in which a bit is ON. such as the hours in which an engine is active.
is it possible to do it with the logic of Geo scada?
is there an internal clock?
can I count the seconds with an internal variable?

How can I create it?

 

I do not have the possibility to modify the device connected to Geoscada, so I have to operate on Geoscada.

 

Thank you all

 

 


Accepted Solutions
AndrewScott
Commander
Commander

Re: Seconds counter

You should be able to do this with a Runtime Accumulator.

https://tprojects.schneider-electric.com/GeoSCADAHelp/Geo%20SCADA%202020/Default.htm#CoreConfigurati... 

 

It shouldn't require a logic program.


Andrew Scott, Lead Engineer, AVEVA

See Answer In Context

2 Replies 2
AndrewScott
Commander
Commander

Re: Seconds counter

You should be able to do this with a Runtime Accumulator.

https://tprojects.schneider-electric.com/GeoSCADAHelp/Geo%20SCADA%202020/Default.htm#CoreConfigurati... 

 

It shouldn't require a logic program.


Andrew Scott, Lead Engineer, AVEVA
Valentino
Ensign Ensign
Ensign
0 Likes
0
575

Re: Seconds counter

Thanks for the help! I solved it using an accumulator