Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84516members
353741posts

Get Telemetry Data without "null"

EcoStruxure Geo SCADA Expert Forum

Find out how SCADA systems and networks, like EcoStruxure Geo SCADA Expert, help industrial organizations maintaining efficiency, processing data for smarter decision making with IoT, RTU and PLC devices.

Solved
abdullah123456789
Lieutenant JG
Lieutenant JG
0 Likes
4
296

Get Telemetry Data without "null"

Hello,

 

I created an SQL Query in Geo SCADA Expert 2021 as in the below.

 

SQL.PNG

 

When I exported the Telemetry Signal List after creating the query, I saw "null" data. This "null" data should not be displayed

 

I did some filtering in this screen in the below but I couldn't be successful. Which filter i must choose?

 

14367827-9709-4ea5-a09a-0a1092c1c32a.jpeg


Accepted Solutions
AndrewScott
Commander
Commander
0 Likes
1
288

Re: Get Telemetry Data without "null"

To filter the resultset of an SQL query based on a column not being NULL use the <column> IS NOT NULL syntax:

https://www.w3schools.com/sql/sql_null_values.asp 

 

The current value of a point is NULL when it has never been updated and the OPC quality will be 'waiting for initial data'.


Andrew Scott, Lead Engineer, AVEVA

See Answer In Context

4 Replies 4
AndrewScott
Commander
Commander
0 Likes
1
289

Re: Get Telemetry Data without "null"

To filter the resultset of an SQL query based on a column not being NULL use the <column> IS NOT NULL syntax:

https://www.w3schools.com/sql/sql_null_values.asp 

 

The current value of a point is NULL when it has never been updated and the OPC quality will be 'waiting for initial data'.


Andrew Scott, Lead Engineer, AVEVA
BGedco2022
Lt. Commander
Lt. Commander
0 Likes
1
265

Re: Get Telemetry Data without "null"

"select x,y, z

from tableName

where x is not null"

To filter a results without null values 

 

OR another filter

 

where x >= 0

AndrewScott
Commander
Commander

Re: Get Telemetry Data without "null"

The correct syntax to exclude NULL values is:

SELECT X, Y, Z FROM TABLE WHERE X IS NOT NULL

 

The following syntax will not work as the SQL standard specifies that the comparison operators (=, <>, >= etc.) cannot be used to test for NULL (see https://www.w3schools.com/sql/sql_null_values.asp😞

SELECT X, Y, Z FROM TABLE WHERE X <> NULL

 


Andrew Scott, Lead Engineer, AVEVA
abdullah123456789
Lieutenant JG
Lieutenant JG
0 Likes
0
176

Re: Get Telemetry Data without "null"

Thanks for help. It worked.