Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84406members
353611posts

.Is the EcoStruxure Automation Expert HMI dynamic or static?

EcoStruxure Automation Expert / IEC 61499 Forum

Browse this forum to find everything you want to know about EAE and IEC 61499 for distributed control systems. Ask experts your questions, get answers, discuss, and share your experience with the growing community.

Rodrigo_Garcia
Administrator Administrator
Administrator
0 Likes
2
1358

.Is the EcoStruxure Automation Expert HMI dynamic or static?

.

Rodrigo G. 


Industrial Automation Community manager

Tags (1)
2 Replies 2
JeromePetit
Ensign Ensign
Ensign
1
1354

Re: .Is the EcoStruxure Automation Expert HMI dynamic or static?

With EcoStruxure Automation Expert all Composite Automation Template  (CAT or object) may/should have their visual facets.

 

This CAT HMI facet represent, most of the time, dynamically the asset state on the HMI synoptic.

 

The HMI facet can include more than just visualization of current state of the asset but also alarms and events associated to this  component as well as archived data such as trends and alarms.

 

From the build in CAT library you can choose between different type of dynamic visualization of your objects with "old fashion" "Green/Red" process representation to more optimal operation methods such as Situation Awareness look & feel.

 

 

EAE Synoptic.jpg

 

 

Tags (1)
Adrianaa
Cadet
0 Likes
0
1181

Re: .Is the EcoStruxure Automation Expert HMI dynamic or static?

Opening the proceedings, Jean-Pascal Tricoire, Chairman and CEO, Schneider Electric, said that we have digitized a number of processes. We are also focusing on climate change. When we are forced to change, we can, as Covid-19 has shown us.  Our mission is to provide digital experience for the customers. We now need to make the world change practically. We also need to find new ways to support customers in new, effective manners.

Tags (2)