Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84257members
353353posts

Is real time possible with IEC 61499?

EcoStruxure Automation Expert / IEC 61499 Forum

Browse this forum to find everything you want to know about EAE and IEC 61499 for distributed control systems. Ask experts your questions, get answers, discuss, and share your experience with the growing community.

Solved
Rodrigo_Garcia
Administrator Administrator
Administrator
3
1310

Is real time possible with IEC 61499?

.

Rodrigo G. 


Industrial Automation Community manager

Tags (1)

Accepted Solutions
JohnConway
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
0
1309

Re: Is real time possible with IEC 61499?

Our measurements with EcoStruxure Automation Expert show that event-driven systems are extremely efficient in terms of resource use, more so than scan-based systems. We are currently running field tests with industrial customers for different applications. Please contact your Schneider Electric Representative to learn more.

See Answer In Context

Tags (1)
3 Replies 3
JohnConway
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
0
1310

Re: Is real time possible with IEC 61499?

Our measurements with EcoStruxure Automation Expert show that event-driven systems are extremely efficient in terms of resource use, more so than scan-based systems. We are currently running field tests with industrial customers for different applications. Please contact your Schneider Electric Representative to learn more.

Tags (1)
RakeshSuresh
Crewman Crewman
Crewman
1
1005

Re: Is real time possible with IEC 61499?

There is a possibility to enable Real-time in IEC61499 using  E_CYCLE Function Block, which can be used as the clock generator. 

Tags (1)
Bram-Marsman
Crewman Crewman
Crewman

A more aRe: Is real time possible with IEC 61499?

The term "real-time" is confused here with cyclic I think.

 

A more accurate description would be that E_CYCLE allows you to do classic cyclic control, which is not the intent off course.

 

However, don't forget cyclic control will always be required.

For time-related computation, such as PID-control or accumulators you will need E_CYCLE even - or I should say especially - when nothing changes / no event occur.

 

Tags (1)