Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84785members
354230posts

Automation Expert SE.AppCommonProcess Motor Deep Dive

EcoStruxure Automation Expert / IEC 61499 Forum

Browse this forum to find everything you want to know about EAE and IEC 61499 for distributed control systems. Ask experts your questions, get answers, discuss, and share your experience with the growing community.

Frank_P
Crewman Crewman
Crewman

Automation Expert SE.AppCommonProcess Motor Deep Dive

The SE.AppCommonProcess library has many excellent features and greatly reduces the need for low engineering type tasks.

 

This also means that there are so many different ways to control a Motor for example.

 

This PDF provides basic examples of the different ways to start and stop the Motor CAT.

 

Enjoy !

Frank_P
Attachments
2 Replies 2
DP-JYC
Lieutenant JG
Lieutenant JG
0 Likes
1
1581

Re: Automation Expert SE.AppCommonProcess Motor Deep Dive

Thank you @Frank_P for sharing this information & examples.

Could you attach examples in an archive here?

Tags (1)
Frank_P
Crewman Crewman
Crewman

Re: Automation Expert SE.AppCommonProcess Motor Deep Dive

Here is a V21.2 Update 1 version of doing local control with a Motor and Valve.

This does not have permissives and or interlocks or remote SP but shows how to setup the items as local control and turning them on and off.

Frank_P
Attachments
Tags (1)