Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Digital Twin

This knowledge base is addressing usage of software Experior, Machine Expert Twin and future Automation Expert Twin. These softwares are used to create smaller instances of digital twins for use in industrial automation, warehouse management, design & engineering with more..
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
  • Digital Twin
  • Digital Twin
  • Label: Exp-6 Getting Started
Options
  • Knowledge Base Article Dashboard
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
  • Alphabetical
  • Experior 6 85
  • Experior 7 57
  • Exp-6 Developer Guide 35
  • Exp-7 Developer 16
  • Exp-6 User Guides 16
  • Exp-7 Communication Protocols 11
  • Exp-6 Experior 11
  • Exp-6 Communication Protocols 11
  • Exp-7 Getting Started 10
  • Exp-6 Dev Environment 9
  • Exp-7 User Interface 9
  • Exp-6 Dev Assembly 7
  • Exp-7 Building Models 6
  • Exp-7 Working With Models 5
  • Exp-6 PLC 4
  • Exp-6 Getting Started 3
  • Exp-7 Importing Graphics 3
  • Exp-6 3rd Party Programs 2
  • Exp-6 Tips and Tricks 2
  • Remote Viewer 2
  • Exp-6 Model Modifications Examples 1
  • Previous
  • 1 of 3
  • Next
Top Contributors
  • Kasper.Vestrup
    Kasper.Vestrup
See More Contributors

Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

Label: "exp-6 getting started"

View in: "Digital Twin" | Community

3 Posts | First Used: 2026-01-09

Digital Twin

Sort by:
Date
  • Date
  • Views
  • Likes
Options
  • Knowledge Base Article Dashboard
  • Subscribe
  • Bookmark
  • Invite a Friend
Label: "Exp-6 Getting Started" Show all articles

Startup Options

On occasion, it can be useful to launch Experior from the command line to change the program’s functionality.   This article details the functionality of each command line argument, that you can use can use when launching Experior.   <file name> Experior opens a model if an argument matches the name of an existing Experior model.   -event Starts Experior in Discrete Events Mode (only functional with the right privileges).   -physics Starts Experior in Physics Mode (only functional with the right privileges).   -menu Hides the main menu (ribbon).   This option can also be toggled within Experior from the main menu or by using F10 providing the -menu switch has not been used when starting Experior.   -comtest Display fetch/write durations.   -tester Startup in ‘Tester’ mode.   -debug Enable ‘Debug’ mode.   -config Display the ‘Catalog Selector’ dialog during startup.   -log <path> Set a temporary log directory (example: c:\Experior\Logs\).   <path> Set working directory (permanently) (example: c:\Experior\).   -reset Reset the Working directory.   A set of options also exists for automated startup and testing of models. These are detailed below. -autostart Run the model when it is loaded. This will only be executed when Experior has finished opening and the model has finished loading and initializing.   -stopafter <dur> Stop the model and close Experior after a period of time – <dur> (duration) defines the time in seconds before the model stops and Experior starts closing.   -atstart <sym/name> Here you provide a symbol name or assembly name that should be activated when a model is started (after connections are established) so that this can initiate some action in the model.   -seed <seed> The seed used by the random generator.   -invisible Start Experior invisible (rendering disabled). Only if <file name> is defined.   -oem Start Experior in OEM licence mode.
View full article
Kasper.Vestrup Explorer
‎2026-01-13 05:46 AM

Labels:
  • Exp-6 Getting Started
  • Experior 6
122 Views

NVIDIA PhysX configuration (relevant in Physics Mode)

(Only relevant in Physics Mode)    Selecting a GPU allows an increase in PhysX processing and will improve overall performance in Experior.  
View full article
Kasper.Vestrup Explorer
‎2026-01-09 12:57 AM

on ‎2026-01-09 12:57 AM

Labels:
  • Exp-6 Getting Started
  • Experior 6
102 Views

Installing Experior 6

Download the required version of Experior Go to the Release folder, open the folder containing needed Experior version and download the setup file. Double click the Experior install file. On the License Agreement screen, select I Agree.   If you want a custom installation path click the Options button. Otherwise click the Install button.   The program will now install, if a User Account Control window appears click YES. Once the installation is complete, click CLOSE to finish.
View full article
Kasper.Vestrup Explorer
‎2026-01-09 12:56 AM

on ‎2026-01-09 12:56 AM

Labels:
  • Exp-6 Getting Started
  • Experior 6
550 Views
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.