New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Loads, Feeder & Eater
Digital Twin
This knowledge base is addressing usage of software Experior, Machine Expert Twin and future Automation Expert Twin. These softwares are used to create smaller instances of digital twins for use in industrial automation, warehouse management, design & engineering with more..
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
The feeder and eater are two elements of a model that are closely connected. The feeder produces loads while the eater ‘eats’ the loads so they disappear from the model again. Read more about them beneath.
Feeder
As mentioned above, the feeder produces loads. Loads represent any product the model is designed to handle, for instance luggage, boxes or trays. If you double click a conveyor, it will produce a load. However, if you want to produce several loads, you will need to use a feeder. In the Physics mode, you can find the feeder in the Experior catalog under conveyors:
In the Discrete Events mode you can find the feeder in the demo catalog. From the catalog you can double click the feeder and place it in the scene. Alternately you can right click on a conveyor you wish to add the feeder to, and choose the ‘insert feeder’ option.
Once you have added a feeder, it will start producing loads when you press play on the model. If you click on the feeder, you will be able to see its properties in the properties window. From here you can see, which type of load you are using as well as change load type under load>type. The default is a package but there are several options to choose from. A graphical overview of the all the available Load types – including the list shown in the image below:
It is also possible to make your own loadtype by uploading your own file. You do this by selecting the loadtype called ‘file’. From here a menu will pop up, where you can upload your own. Besides showing the load type, the properties window for the feeder holds other information such as the loads size or any barcode connected to the loads. It is also possible to set a time interval for how often the feeder should produce a load. Alternately you can instruct the feeder to produce a new load when the previous load is a specified distance away from the feeder.
Supported File Formats
.x (Microsoft DirectX)
.dae (COLLADA)
.fbx (Autodesk FBX)
.obj (Wavefront)
.3ds (Autodesk 3D Studio)
.ase (Autodesk 3D Studio ASCII)
.stl (Stereolithography)
.lwo (LightWave)
.dxf (AutoCAD dxf)
.glb 2.0 (binary)
.gltf (embedded)
Eater
The eater only exists in Physics mode. You will find it under the sensor catalog>misc.>eater:
When a load hits the eater, the load will get ‘eaten’ and disappear. In the properties window you can see the properties for your eater and change its size, visibility etc.
Linking a feeder and an eater
It is possible to link an eater and a feeder to each other. For instance if you have build only parts of your model but still miss some functions, you can set it up so an eater eats the loads in one part of the model and then sends them directly to the feeder in another part of the model, making it possible to circumvent the part of the model, you have not yet build. If you wish to do this, you must go to the properties window of both the feeder and the eater in turn and enable the handover connection box:
You also have to make sure that the port-numbers are a match and the computer does not already use this port – otherwise you will not be able to connect the two. When you have chosen matching port-numbers, that are not already in use, the feeder and eater will connect.
If you wish to connect a feeder and an eater that are not on the same device – for instance you have part of the model open on your computer, your colleague has another on his – it is possible to do so as well. You just need to make sure that the IP address in the properties for the eater matches the IP address of the device, the feeder is on. Then you can connect them.