Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
This knowledge base is addressing usage of software Experior, Machine Expert Twin and future Automation Expert Twin. These softwares are used to create smaller instances of digital twins for use in industrial automation, warehouse management, design & engineering with more..
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
This guide will cover constructing a model, adding controls and controllers, setting up PLC Inputs and Outputs on the components that need them and finally running and testing the model.
In this article a simple model using standard Experior components will be built and the guide will provide more information on some of the properties used by those components.
This is a screen-shot of what the model looks like when finished. Note the tracks are gold because they are locked in place.
Now some basic controls need to be added to the model.
The Control Panel is located directly below the Catalog/Communications pane.
Some of the items in the model have yellow triangles with exclamation marks in them next to them.
The reason for this is because the items or controls are waiting to be linked to a PLC and have either an Input or an Output associated to them.
For the purpose of this exercise three methods for testing inputs and outputs within Experior will be covered. These can be used as a temporary stopgap if you don’t have a PLC, SoftPLC or Controller available for testing. Click on the desired method, follow the guide and return to this guide when ready to run the simulation:
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.