Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Allen Bradley Communication

Digital Twin

This knowledge base is addressing usage of software Experior, Machine Expert Twin and future Automation Expert Twin. These softwares are used to create smaller instances of digital twins for use in industrial automation, warehouse management, design & engineering with more..
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
  • Digital Twin
  • Allen Bradley Communication
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Kasper.Vestrup
    Kasper.Vestrup

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Digital Twin
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
154 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Allen Bradley Communication

Kasper.Vestrup Explorer
‎2026-01-09 01:36 AM

Experior communicates with Allen Bradley PLCs through the CIP protocol. The CIP protocol works by sending tables of data between Experior and the PLC. The datatype of these tables can be BOOL, SINT, INT, DINT or BIT64.

 

The PLC must have corresponding tables that contain the same datatype. At the start of the scan the values of PLC input tables can be mapped over to the correct variables in the PLC program. At the end of the scan the relevant output values can be mapped to the output tables.

 

The advantage of this approach is that input and output values will not change mid-cycle.

 

Experior Setup 

  • First right-click in the communication panel and select EtherNet/IP – CIP

selectCip.png

 

  • Select the connection. The properties for the connection will be shown in the properties window
  • The property of interest is the Size property. This property defines the data type of the tables for this connection. The corresponding tables in the PLC must be of the same datatype

cipDataTypes.png

 

  • Next create a lamp and a button in the Control Panel. Select the lamp

allenBradley3.png

 

  • The properties window will either have a category called PLC Input or PLC Output (depending on if you chose the lamp or the button).

propertiesLamp.png

 

The Connection id property defines which connection is being used.
Slot defines what table is being used. In this case Local_1, can be changed to anything.
Address defines what entry of the table is being used (starting from 0).
Bit No. defines that bit of the selected Address will be used (starting from 0). Bit No. can only be chosen for PLC input/outputs that are of the type bool.

 

  • Set a value for the Address and Bit No. Do the same for the other component in the Control Panel.

 

PLC setup
Each table that is created in Experior has two corresponding tables in the PLC – one for inputs and one for outputs. This means that in the button and lamp example, both can use the same Address and Bit No. in the same table since they will be sent/received from two separate tables in the PLC.
Experior will expect the PLC to have tables corresponding to the tables that are in Experior. The tables in the PLC must be names as follows:

 

Exp_datatype_Input_Experior table name
Exp_datatype_Output_Experior table name

 

 
allenBradley5.png

An example in Studio 5000

Labels (2)
Labels:
  • Exp-6 PLC
  • Experior 6
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.