Issue
What does Accuracy and Resolution mean when mentioned in the Datasheet of a controller with a airflow sensor
Environment
B3-865
B3-866
B3-885
Cause
Need definition of the meaning of Accuracy and Resolution when mentioned in the datasheet of a controller with an airflow sensor
Resolution
Accuracy is the amount that the measurement could be “off” from true reading, either above or below. Resolution is the smallest change that can be detected.