Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Using Digital Point Cards (DPC‑3‑1 / DPC‑3‑2) with a Network 8000 MicroZone II Controller

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Using Digital Point Cards (DPC‑3‑1 / DPC‑3‑2) with a Network 8000 MicroZone II Controller
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • CraigEl
    CraigEl

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2269 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Using Digital Point Cards (DPC‑3‑1 / DPC‑3‑2) with a Network 8000 MicroZone II Controller

Product_Support
‎2018-09-07 04:19 AM

Last Updated: CraigEl Champion ‎2026-03-02 10:37 PM

Issue

Guidance on how to configure and use digital point cards with a Network 8000 MicroZone II controller.

Product Line

TAC IA Series

Environment

  • Network 8000 MicroZone II controller
  • Digital Point Card

Cause

MicroZone II controllers do not natively interpret the digital input signals from DPC‑3‑1 and DPC‑3‑2 cards. A custom application file is required for these cards to function correctly.

Resolution

To enable digital input support on a MicroZone II controller:

  1. Download and load the custom application file
    Use the attached application file 1‑DPC3.MZ2. This file enables the controller to correctly process signals from the DPC‑3‑1 and DPC‑3‑2 digital point cards.

  2. Refer to the attached technical bulletin
    The attached TB01‑26 document provides detailed information on:

    • Supported digital point card models
    • Hardware installation
    • Wiring considerations
    • Application behavior and configuration steps
  3. Compatibility note

    • DPC‑3‑1 and DPC‑3‑2 are the only digital point cards supported by the MicroZone II controller.
    • DPC‑5 series cards were designed for MNL and MNB controllers. They can be used with the DUI Expander Object, but not with standard MicroZone II applications.

(Note: The DPC-5 series cards were designed for the MNL and MNB controllers.  They are compatible with the DUI Expander Object available for both controller lines.)

Labels (1)
Labels:
  • TAC IA Series
Attachments
1-DPC3.zip
Tags (3)
  • Find more articles tagged with:
  • 3189
  • CraigEllis23
  • CraigEllis26
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.