Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

SQL Server using high memory on Security Expert system

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • SQL Server using high memory on Security Expert system
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • AdamSteele
    AdamSteele

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
2 Likes
189 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

SQL Server using high memory on Security Expert system

AdamSteele Champion
‎2026-06-15 07:53 PM

on ‎2026-06-15 07:53 PM

Issue

SQL Server is observed consuming almost all of the memory on a system configured with 64GB RAM, with memory utilization reaching around 85–94%. This appears high compared to the recommended 32GB baseline for Security Expert.

Product Line

EcoStruxure Security Expert

Environment

  • Security Expert Client Server
  • SQL Server

Warning

Potential for Data Loss: The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure or unfamiliar with any complex steps detailed in this article, please contact Product Support for assistance.

Cause

Microsoft SQL Server is designed to aggressively consume available system memory to optimize performance when the max server memory limit is not explicitly configured. On Security Expert systems with higher RAM capacity, this behavior can appear abnormal when compared to minimum sizing guidance, even though it is expected SQL Server operation.

Resolution

This behavior is normal and expected.

  • SQL Server is designed to aggressively use available memory to maximize performance (for example, buffer pool and query plan cache). If the max server memory setting is not configured, SQL Server can consume approximately 80–95% of available RAM and will only release memory when the operating system is under pressure.
  • The 32GB RAM recommendation defined in the SX-SRVR Security Expert - Client Server - Installation Guide should be considered a minimum baseline, not a maximum limit. Larger systems with more controllers, events, integrations, and historical data may require significantly more memory.
  • If it is necessary to limit SQL Server memory usage (for example, to 70–80%), configure the max server memory setting accordingly. For example, on a 64GB server, setting the limit to approximately 48GB allows sufficient RAM for the operating system.
  • If performance degrades after applying a memory limit, this indicates that additional RAM may be required. In such cases, increasing total system memory and adjusting the SQL Server limit is recommended.
  • The max server memory setting can be configured in SQL Server Management Studio under server properties (Memory tab) or via T-SQL using sp_configure. Changes are applied immediately and do not require a restart. See Server memory configuration options Microsoft article for further details.
Labels (1)
Labels:
  • EcoStruxure Security Expert
Tags (1)
  • Find more articles tagged with:
  • AdamSteele26
Was this article helpful? Yes No
100% helpful (2/2)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.