Issue
Installers occasionally use the Analog Output (AO) of Xenta controllers to operate external relays. This approach is typically adopted when additional discrete on/off control points are needed, and the AO channels are not required for proportional control.
Product Line
TAC Vista
Environment
- Xenta programmable controllers
- Xenta 281, 282, 283, 301, 302, 401
Cause
This method is often chosen to avoid the cost of upgrading to higher-capacity controllers or adding Xenta I/O expansion modules. The implementation usually involves:
- Connecting a 12V DC relay to the AO output.
- Setting the AO to 100% (10V) to energize the relay.
- Setting the AO to 0% (0V) to de-energize the relay.
Resolution
Although this use of AO for relay control is not recommended in standard designs, it can be implemented reliably if the following considerations are addressed:
- Relay Selection: Ensure the relay is compatible with the AO voltage and current characteristics.
- Installation Practices: Proper wiring, isolation, and protection should be applied to prevent damage or erratic behavior.
- Controller Configuration: Confirm that the AO channel is correctly programmed to deliver the required voltage levels.
For detailed guidance, refer to the document:
📄 Xenta Analog Output WP-001.040804.pdf