Issue
There seems to be no way to delete the photo in a personnel object.
Environment
CyberStation
Cause
Keep the personnel object and delete the photos in the personnel object.
Resolution
There is no way to delete the photo once it has been captured into the personnel object, a workaround is to create a blank image using an application such as Windows Paint for example and then change the personnel’s photo to the blank image.