Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Execution Precedence Sets Program Execution Order but Not Priority

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Execution Precedence Sets Program Execution Order but Not Priority
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo
  • DavidFisher
    DavidFisher
  • PaulFr
    PaulFr
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2391 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Execution Precedence Sets Program Execution Order but Not Priority

Product_Support
‎2018-09-06 11:59 AM

Last Updated: RobertAndriolo Champion ‎2026-08-17 09:51 PM

Issue

  • Can Execution Precedence be used to determine the priority of a program that is bound to a value?
  • Application Task shows the "Conflicts" property set to true
    ApplicationSchedulerTask3.png
  • High Memory/CPU values causing performance issues with Automation Servers running a large number (100+) of applications (Function Block Programs and Script Programs) 

Product Line

EcoStruxure Building Operation

Environment

  • Building Operation Automation Server (AS. AS-B, AS-P, AS-P-3) 
  • Function Block programs
  • Script programs

Cause

The behavior of the Execution Precedence property is often misunderstood. Execution Precedence is intended to help the Application Scheduler establish a valid execution sequence between dependent programs. It does not provide a program priority mechanism and cannot be used to determine which program has control of a value when multiple programs are bound to the same output. Incorrect assumptions about its purpose can result in dependency-cycle issues, application conflicts, or unexpected control results

Resolution

Execution Precedence is a program property available in both Function Block and Script programs. It is configured from the program Properties on the Basic tab.

How Execution Precedence Works

Execution Precedence controls the order in which programs are executed.

  • Programs with lower Execution Precedence values execute before programs with higher values.

Program execution is coordinated by the Application Scheduler. For synchronized tasks, the scheduler normally determines execution order by analyzing dependencies between program inputs and outputs.

  • Applications that provide data are generally executed before applications that consume that data.

Programs with the Same Execution Precedence

If multiple programs have the same Execution Precedence value, Execution Precedence does not establish an execution-order preference between them.

In this situation, the Application Scheduler determines the execution order based on program dependencies.

Important: Programs with equal Execution Precedence values should not be assumed to execute in a specific order unless that order is defined by their dependencies.

Using Execution Precedence for Dependent Programs

Execution Precedence can be used when one program generates a value that is required by another program.

Example

  • Program A calculates a compensated setpoint.
  • Program B is a PID control program that uses the compensated setpoint as its reference value.
  • Program B must have a higher Execution Precedence value than Program A so that the compensated setpoint is calculated before the PID program executes.

Resolving Dependency Cycles

A dependency cycle occurs when two or more programs depend on each other, preventing the Application Scheduler from determining a valid execution order.

Example

DependencyCycle.jpg

To resolve a dependency cycle:

  1. Identify the program that should execute first.
  2. Assign that program a uniquely lowest Execution Precedence value.
  3. The Application Scheduler uses that value to establish a valid execution order.

Example

  • Program A: Execution Precedence = 10
  • Program B: Execution Precedence = 20

DependencyCycle-Resolution.jpg

Result:

  • Program A executes first.
  • Program B executes second.

Note: If multiple programs within the dependency cycle share the same lowest Execution Precedence value, Execution Precedence does not provide a tie-break mechanism and cannot be used to resolve the cycle.

What Execution Precedence Does Not Do

Execution Precedence affects execution order only.

It does not affect program priority.

If two programs are bound to the same value output, both programs attempt to control that value, resulting in an indeterminate outcome.

Combining Outputs from Multiple Programs

When outputs from multiple programs must be combined, use appropriate logic.

Binary values

  • AND
  • OR
  • XOR
  • Other logical operators

Analog values

  • Maximum
  • Minimum
  • Average
  • Other methods appropriate for the application requirements

References
EcoStruxure Building Operation WebHelp:

  • Application Scheduler
  • Program Cycles in EcoStruxure Building Operation Software
  • Script Programs

 

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (2)
  • Find more articles tagged with:
  • 11172
  • RobertAndriolo26
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.