Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Configuring Access Expert to use PIV cards with AX-SSC using AC1 downstream devices

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Configuring Access Expert to use PIV cards with AX-SSC using AC1 downstream devices
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • AbeMeran
    AbeMeran

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
864 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Configuring Access Expert to use PIV cards with AX-SSC using AC1 downstream devices

AbeMeran Mentor
‎2025-11-02 06:50 PM

on ‎2025-11-02 06:50 PM

Issue

Guidance is needed to enable reading of PIV (FIPS-201) cards using the AX-SSC controller and AC1 downstream devices within EcoStruxure Access Expert.

Product Line

EcoStruxure Access Expert

Environment

AX-SSC

Cause

Sites migrating from Continuum systems require a clear, step-by-step process to ensure PIV cards are properly enrolled and recognized in Access Expert.

Resolution

What is FASC-N?

FASC-N stands for Federal Agency Smart Credential Number. It is a 25-byte (200-bit) identifier embedded in PIV cards, used to uniquely identify the cardholder across federal systems. It is composed of multiple fields, including:

  • Agency Code
  • System Code
  • Credential Number
  • Credential Series
  • Credential Issue
  • Person Identifier
  • Organizational Category
  • Organizational ID
  • Person Org Association

These fields are encoded using Packed Binary Coded Decimal (BCD) with odd parity, and together form a unique string used by access control systems to authenticate users.

Understanding the FASC-N Structure

In the Continuum Personnel object below, the fields highlighted are those that make up the FASC-N

AbePIVAnotated.JPG

The PIV enrollment tool generates a character string when a card is presented. For example:

32013733334894141152472674132011

This string is composed of the following FASC-N fields:

Field Value
Agency Code 3201
System Code 3733
Credential Number 334894
Credential Series 1
Credential Issue 4
Person Identifier 1152472674
Organizational Category 1
Organizational ID 3201
Person Org Association 1

Note: If no enrollment tool is available, manually concatenate these fields in the order shown to create the FASC-N string.


Configuration Steps

1. Card Format Setup

Configure the card format in Access Expert as follows:

  • Card Format Type: Standard
  • Bit Length: 128
  • Large Encoded Card Number: ✅ Checked
  • Convert 200 FASCN Bit to 128 Bit: ✅ Checked
  • Card Number Starting Bit: 0
  • Card Number Bit Length: 128

    CardFormat.JPG


2. AX-SSC Controller Configuration

  • Ensure Enable Large Encoded Card Number is checked.
  • Assign the card format created in Step 1 to the controller.

    AX-SSC.JPG


3. Person Object Configuration

  • Navigate to Add Card Assignments.

    Galileo2.JPG

  • Paste the full FASC-N string into the Display Card Number field. This will auto-populate the Encoded Card Number field.

  • Since the Encoded Card Number field is limited to 16 characters, truncate the string from the end until only 16 characters remain.

  • Paste the full FASC-N string into the Hex Value field.

    CardAssignment.JPG

    ⚠️ Although labeled "Hex Value", enter the string as decimal digits.

  • Save the Person object.


Additional Notes

  • Only the editors mentioned above require configuration for PIV card support.
  • Editors such as Reader, Access Level, etc., do not need special configuration for PIV cards.
Labels (1)
Labels:
  • EcoStruxure Access Expert
Tags (1)
  • Find more articles tagged with:
  • AbeMeran25
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.