Issue
WorkPlace Tech or WorkPlace Tech Editor does not start, does not function correctly, or fails to load expected components such as the WorkPlace Tech ribbon.
Examples may include:
- WorkPlace Tech fails to launch
- WorkPlace Tech Editor ribbon does not appear in WorkStation
- Application starts but does not function correctly
- Errors occur during startup
Product Line
TAC IA Series, EcoStruxure Building Operation
Environment
- WorkPlace Tech Editor (Foresight/EBO Workstation)
Cause
Workplace Tech can have issues caused by:
- uninstall/re-install
- converting from 32-bit Visio to 64-bit Visio
- Conflicts with existing software, like Studio360 - WorkPlace Tech Editor Ribbon Fails to Load When Launching WorkStation or WorkPlace Tech
- Windows permissions during installation or runtime environment
Resolution
Collect debugging files to submit to Product Support for review.
- Create the Windows Temp folder if it does not exist. C:\TEMP, C:\Temp, and C:\temp are all considered the same directory.
- Add the following files:
- Debug.txt
- DebugWPT.txt
- Launch WorkPlace Tech or WorkPlace Tech Editor (from Workstation), and proceed until failure condition is displayed.
- Collect those two files and provide to PSS along with summary of the process from launch to failure.