Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84245members
353345posts

StruxureWare Power Monitoring Expert 7.2 Cumulative Update 2

Archives: Power Management Systems

Kevin_Huang
Spock Spock
Spock

StruxureWare Power Monitoring Expert 7.2 Cumulative Update 2

StruxureWare Power Monitoring Expert (PME) 7.2 Cumulative Update 2

Please Read First:

  • Cumulative update should be installed on all PME Setup Types, such as Standalone Server, Database Instance, Primary Server, Secondary Server, Engineering Client and Reporting Client Only
  • is ONLY for PME 7.2 system, NOT SPM or ION Enterprise system
  • is neither a service pack nor a new version of PME
  • contains NO new features but a collection of hotfixes that Continuous Engineering packages and recommends for PME 7.2 system
  • will be a regular part of our application lifecycle moving forward.

What is in PME 7.2 Cumulative Update 2?

  • Hotfix 21829 - It is no longer necessary to run reports in order to save them
  • Hotfix 20348 - Improves performance of the ION Power Quality Aggregator service
  • Hotfix 21473, 21464 - Corrects Dashboards/Reports source selector display issues in systems that have an extremely large number of nodes
  • Hotfix 19241 - Corrects the problem where in some systems the System Log shows excessive ‘Site Connected’ events
  • Hotfix 21792 - Corrects the problem where device names that included Chinese characters would not display in Diagrams
  • Hotfix 21958 - Corrects the problem where jpg images with a space in either the file name or the path to the files would not display in Diagrams
  • Hotfix 21748 - Corrects the problem where custom labels assigned in Vista diagrams would not display in Diagrams
  • Hotfix 21520 - Corrects an issue where device licenses were counted incorrectly in some cases
  • Hotfix 21945 - Adds ACCESS 9xxx devices to offsite.xml to allow offline configuration of these device types
  • Hotfix 21962 - Corrects an issue where the billing report hierarchy templates could not be uploaded
  • Hotfix 21830 - Improves the load time of the report list when it contains a large number of licensed reports
  • Hotfix 22172 - Corrects a possible Log Inserter performance problem in systems which include Micrologic Compact NSX device types
  • Hotfix 21803 - Corrects an issue where it was not possible to run the OPC Server Assistant in Designer
  • Hotfix 21438 - Corrects a possible issue with the Hierarchy Manager when it is used in time zones that are ahead of GMT

Who should get PME 7.2 Cumulative Update 2?

It is recommended that customers with PME 7.2 system should download and installthis update to get the latest hotfixes for their system.

 
How to install PME 7.2 Cumulative Update 2?

  1. Make sure you have PME 7.2 installed on your Standalone server and you have administrative access on the servers
  2. Download the PME 7.2 Cumulate Update 2 (PME 7.2 Cumulative Update 2.exe) to your Standalone server
  3. Run the PME 7.2 Cumulate Update 2 locally on your Primary server and follow on-screen instructions
    - Cumulative Update install may require stopping and restarting services to update the system
    - Cumulative Update install may recommend a reboot after installation if some files were locked and couldn't be replaced
  4. After the PME 7.2 Cumulate Update 2 is installed successfully, installed hotfixes will be shown in your Window's registry
    - if you have 64bit Windows,HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\ION Enterprise\7.2\Cumulative Updates
    - if you have 32bit Windows,HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\IONEnterprise\7.2\Cumulative Updates
  5. Repeat step 1 to 4 on your Database Instance
  6. Repeat step 1 to 4 on your Primary server
  7. Repeat step 1 to 4 on your Secondary server
  8. Repeat step 1 to 4 on your Engineering Client
  9. Repeat step 1 to 4 on your Reporting Only


Kevin Huang
PME Global Offer Manager

Click here to learn more on how PME helps you improve electrical safety, power reliability, operation efficiency and regulation compliance of your facility.
Attachments