Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84342members
353519posts

PME 8.1 Vista feature request

Archives: Power Management Systems

sesa197217_brid
Ensign Ensign
Ensign

PME 8.1 Vista feature request

I've recently been working with a customer who would like to see Numeric and Status objects automatically re-size themselves based on the dimensions of a custom graphic.  For example, if a jpeg image is selected to be used with a Status object a check box would be present in the setup window for the option to "Size to custom image dimensions".  If the jpeg used is 200 pixels wide by 300 pixels in length this would adjust the size of the status object without having to manually.