Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84563members
353833posts

PME 7.xCE Driver AccuSine PCS Broad Spectrum Firmware

Archives: Power Management Systems

Matt_Curry
Administrator Administrator
Administrator

PME 7.xCE Driver AccuSine PCS Broad Spectrum Firmware

Description:

AccuSine_PCS Custom Edition Driver for PME 7.x.  It only contains a set of real-time registers in the driver for AccuSine units with firmware version v7 (DIM Emulator) and v8 (first digital version with DIM emulator).  The package contains default diagrams, and PC logging can be set up on these device drivers.  The manifest release document shows the available mappings for this driver.

Details about AccuSine HMI and Control Board FW versions:

  • HMI V2.xx with V7.yy firmware emulates DIM in display. All have 30000 series registers for Modbus - may not be compatible with a lot of Modbus uses.  (Magelis XBTGT1135 series HMI is used.)   [Upgradable . Requires software upgrade to HMI V4.xxx  new control board (firmware V9.yy), and new communications cables (between HMI and Control board).] 
  • HMI V3.xxx is fully digital.  Compatible with V8.yy firmware.  Has 30000 series registers for Modbus.  Does not display data for 2nd - 49th harmonic data nor have registers for same. [Upgradable by loading HMI V4.xx software and replacing control board with V9.yy firmware.] [Upgradable to color HMI V4.xx by replacing HMI, comms cable, and control board.] 
  • All HMI V4.xx are backward compatible to units with  V8.yy firmware.  Color monitor included. Firmware V8.yy has 30000 registers and does not display 2nd to 49th harmonic orders.

Availability:

AvailabilityRestrictions
Power Monitoring Expert 7.x
  • No official technical support
  • English only
StruxureWare Power Monitoring Expert 7.0.1
  • No official support technical support
  • English only

Price:

Free

Content Creator:

Schneider Electric

Contact Information:

n/a

Technical Support:

This driver is not supported through standard support channels.  It is provided in an as-is state.  By downloading this package you are agreeing to the terms and conditions listed below.


Terms and Conditions:

Please select below to review terms and conditions

Download:

Download package available on Box at the following location:

https://schneider-electric.box.com/s/63ybeh8llmnp8jh30puy

2 Replies 2
sesa252887_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
20

Re: PME 7.xCE Driver AccuSine PCS Broad Spectrum Firmware


Hi Matt,

Thanks for your detailed illustration.

But I do not see any file name with accusine in the folder.

Is there another name for Accusine?

Thanks

Matt_Curry
Administrator Administrator
Administrator
0 Likes
0
20

Re: PME 7.xCE Driver AccuSine PCS Broad Spectrum Firmware

Hi Abon,

Do you see the other drivers in the folder?  It is listed as Accusine PCS just below the ABB RTU 2000.  If you have any issues still, let me know and I can send you the driver package directly.