Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84519members
353747posts

Multiple PME connected to single server with multiple SQL instances

Archives: Power Management Systems

Charles_Murison
Picard Picard
Picard

Multiple PME connected to single server with multiple SQL instances

Would it be possible to test the condition of having multiple PME application servers talking to a single SQL database server. Each application would have it's own Instance within SQL.

L4 Prime for Advanced metering and Utilities
1 Reply 1
Attila_Fritz
Spock Spock
Spock
0 Likes
0
29

Re: Multiple PME connected to single server with multiple SQL instances

I think this is already possible in a minimalist architecture as long as each PME installation has its own SQL instance to reference.