Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84586members
353853posts

Connect an EGX300 with Energy Opertation via a GPRS modem

Archives: Power Management Systems

Solved
JWdenBraber
Ensign Ensign
Ensign
0 Likes
10
1376

Connect an EGX300 with Energy Opertation via a GPRS modem

Hello,

does anyone have a manual and/or experience how to connect an EGX300 to EO via a GPRS modem? And if possible with a SE modem (like the Wavecom).

kind regards,

Jan Willem

Tags (4)

Accepted Solutions
dborle
Lt. Commander
Lt. Commander
2
1129

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

Hi Jan Willem,

I suggest to use the Digi WAN GPRS modem which is also used for SEMS applications. It works very well together with the EGX300. I did some tests for remote access to the EGX300 and devices behind it. As we have the problem of changeing IP-addresses of the modem when we are working over GPRS (to get a fix address is very expensive, here) we are communicating over DynDNS.

I made a little instruction on how to configure the Digi WAN for our application and made a little try for EO export, what works fine. Please find the instruction here after. If you need more information about the Digi WAN, please feel free to contact me.

Cheers

Daniel

See Answer In Context

Attachments
10 Replies 10
dborle
Lt. Commander
Lt. Commander
2
1130

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

Hi Jan Willem,

I suggest to use the Digi WAN GPRS modem which is also used for SEMS applications. It works very well together with the EGX300. I did some tests for remote access to the EGX300 and devices behind it. As we have the problem of changeing IP-addresses of the modem when we are working over GPRS (to get a fix address is very expensive, here) we are communicating over DynDNS.

I made a little instruction on how to configure the Digi WAN for our application and made a little try for EO export, what works fine. Please find the instruction here after. If you need more information about the Digi WAN, please feel free to contact me.

Cheers

Daniel

Attachments
JWdenBraber
Ensign Ensign
Ensign
0 Likes
1
1129

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

Hi Daniel, Thanks for your reply. Is the Digi Wan a Schneider product? Or do you have some specs so we can search a local provider?

dborle
Lt. Commander
Lt. Commander
0 Likes
0
1129

Re: Re: Connect an EGX300 with Energy Opertation via a GPRS modem

This is a product, which I think it's not from Schneider, but it is referenced in our catalogue. Here is the catalogue page from the Simple Energy Management Solutions catalogue. You have 2 references:

1. METEGGNI which is only the modem

2. METEGGXI the modem which is delivered with an EGX300

Attachments
sesa236671
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
1129

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

Some info buried near the bottom here:

http://energyoperation.info/

sesa5886
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
1129

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

We also use the combination of EGX300 + DIGI WAN Modem + EO in our project (with success). The configuration of DIGI Wan and EGX300 is decribed in the attached document (page 103).

Attachments
sesa242973_brid
Ensign Ensign
Ensign
0 Likes
0
1129

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

sorry just call our supplier, DIGI WAN is end of life................

end of this year is a other model avalible.

someone experience with MOXA?

LaurentCoene
Captain Captain
Captain
0
1129

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

Hi Jan,

Many countries are using the InHand 701 3G industrial router.

It goes for $180 fob Beijing and works really well!

We have used it in HongKong, China, South Africa, New Zealand...

It's a lot cheaper than the Digi!

Having said that there are many other options out there!

In the end you should start using the Com'X200 though.

🙂

JamesJeanette
Commander Commander
Commander
0 Likes
2
1129

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

Global System for Mobile Communications - Installation Guide for EGX300 with Digi WAN.

Attachments
sesa102207
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
1129

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

Hi ,

The doc you posted is very helpful. However, it looks like it is from 2010.  The FTP information for REM/EPO/EVO is out of date.  To push data to REM, you must now always connect to 72.2.4.41.  The previous domain as shown in the doc on page11, epo.energyinteractive.com has been decommissioned.

JamesJeanette
Commander Commander
Commander
0 Likes
0
1129

Re: Connect an EGX300 with Energy Opertation via a GPRS modem

Yes...that is an older document. Let me see if we can have it updated.

Thanks