Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84269members
353375posts

Kickstarting home automation

Archives: Power Distribution

VictoriaSwift
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
2
695

Kickstarting home automation

Research has shown that smart energy is the key driver for the connected home, taking priority over security, entertainment and appliances like smart fridges.

 

A smart heating system is often the first step that homeowners take towards home automation, with the integration of further smart devices such as lights and alarms following later.

But why is heating proving to be such a popular initial step towards the smart home?

Rewards Marketo Campaign Images - 14.jpg

 

 

Friendly and familiar

 

While there is still much apprehension around some smart technology, the concept of smart heating is already becoming familiar territory for homeowners. Controlling heating via your phone is now commonplace, as manufacturers and even energy companies themselves develop and promote their own systems.

 

Fuss-free installation


With no need for any re-wiring, smart heating systems are one of the quickest and simplest ways to add automation to any home. Many systems come with industry standard UK wallplates, allowing installers to simply switch a traditional thermostat for a smart one. The system is up and running as soon as the controls are commissioned.


Enhanced convenience


Smart heating offers the convenience of controlling a property’s temperature and hot water from a smartphone, anywhere in the world. When plans change, heating schedules can be changed too. It’s also ideal for remotely monitoring heating at a second property – whether that’s a holiday home, or an elderly relative’s house.


Personalised room control


Thanks to innovative additions like smart radiator thermostats, it’s easier than ever to create designated ‘heating zones’, allowing users to take their smart home to the next level and control heating on a room-by-room basis.

 

If your customer is cold in bed, they can switch the heating on only in the room they are occupying, without the need to heat the whole house - or even get out of bed! Maybe they have a baby who needs to be kept at a specific temperature, or they want to dry some washing in the spare room – it’s all simple with smart radiator thermostats.


Energy savings


Over 80 per cent of domestic energy consumption is used on heating and hot water (DECC 2013) – that’s more than quadruple the amount spent on lights, tumble dryers, washing machines, cookers and televisions put together.

Smart heating systems not only offer convenience; they also offer significant cost savings by not wasting energy.

 

When used effectively, a multi-zone system offers the potential to save significantly over a smart thermostat system alone.

 

There is also the added benefit of being able to more accurately control the temperature, as reducing it by just one degree can save the homeowner money on their bill.

 

The Wiser choice


With this in mind, Drayton by Schneider Electric have developed Wiser, an affordable smart heating system with four key components; the Heat Hub, the room thermostat, radiator thermostats, and the app.

 

This new offering boasts speedy installation, with an industry standard UK wallplate on the Heat Hub allowing Wiser to be retrofitted in minutes. The system also boasts a simple interface through which multiple users can easily control up to three channels, 16 zones and 32 devices with the use of one intuitive app. Wiser is also compatible with Amazon Alexa, enabling full voice control.

 

Wiser Approved Installer 3.jpg

 

To become an expert in Wiser installation, configuration and maintenance, you can complete a CPD approved training course to become a Wiser Approved Installer. This will give you access to an Approved Installer badge and further benefits, helping you to build trust with customers.

 

 

Victoria Swift
Digital Marketing Specialist
Tags (1)
2 Replies 2
CharlieKnight
Lieutenant JG
Lieutenant JG
0 Likes
0
646

Re: Kickstarting home automation

How long does the Wiser Installer training take?

VictoriaSwift
Lieutenant JG Lieutenant JG
Lieutenant JG

Re: Kickstarting home automation

Hi @CharlieKnight - the training takes around 40 minutes.

Victoria Swift
Digital Marketing Specialist