Posted:
2016-02-05
07:23 AM
. Last Modified:
2021-11-23
11:13 PM

- Multiple single-sensor cameras can be replaced by one Optera camera.
- Optera fills the gaps in coverage that no number of single-sensor cameras can fill. Optera provides TOTAL situational awareness.
- With one camera and one cable, you can install Optera with lower costs and minimal impact to the building aesthetics.
- Fewer Optera cameras save VMS license costs with only one license per Optera camera.
- You don’t need to hire someone to actively do surveillance. With Optera, you can record and view video whenever you want.
- Optera’s fewer mechanical parts reduces maintenance costs compared to PTZ cameras.
- Operators have limitations on the number of cameras they can effectively monitor. Optera increases the area covered using a fewer number of cameras.
- Most of Optera’s 8 analytic behaviors span the entire panoramic scene.
- Optera cameras cost less than PTZ cameras with comparable image quality.
- Optera simultaneously adjusts to lowlight and WDR throughout the entire 180°, 270°, and 360° scene to maintain evidentiary detail.