Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84814members
354267posts

Recording BOSCH and FLIR cameras

Archives: Industrial Automation and Control

Solved
sesa249628
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
85

Recording BOSCH and FLIR cameras

Hi I have Endura Express, One BOSCH Camera and one FLIR Camera connected to a network. BOSCH and FLIR are  connected through Pelco Encoder. I'm able to see live video for both the cameras but recording status is showing error in Endura utilities. Do these cameras require additional hardware(eg. UDI) to enable recording?


Accepted Solutions
Kly
Sisko
Sisko
0 Likes
0
25

Re: Recording BOSCH and FLIR cameras

If cameras are connected through Encoder, they are analog. Do you mean NET5402T as Encoder. If so, you need to add Cameras to Recording through Web-interface of Endura XPress. After that you should configure Recording Schedule through WS5200 Software.

You do not need additional Hardware for analog cameras except encoders.

See Answer In Context

1 Reply 1
Kly
Sisko
Sisko
0 Likes
0
26

Re: Recording BOSCH and FLIR cameras

If cameras are connected through Encoder, they are analog. Do you mean NET5402T as Encoder. If so, you need to add Cameras to Recording through Web-interface of Endura XPress. After that you should configure Recording Schedule through WS5200 Software.

You do not need additional Hardware for analog cameras except encoders.