Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84654members
354004posts

Endura Systems compatible with Evolution cameras (Panoramic)

Archives: Industrial Automation and Control

harry_scovel
Crewman
Crewman

Endura Systems compatible with Evolution cameras (Panoramic)

Wondering if there are problems with adding the Evolution cameras to an existing Endura system. Will they work without additional software and what is the average record space needed per camera?

Thanks

1 Reply 1
steven_berg_vb_
Lieutenant
Lieutenant

Re: Endura Systems compatible with Evolution cameras (Panoramic)

Harry,

This is what I have found in testing a 360' evolution camera.

- Need a UDI to decode the ONVIF video. Not plug and play with Endura.

- Only get 1 Stream. I am only able to see it full screen (Single pane). Any multiple panes did not work.

- Able to record, but remember, only full warped 360' view.

- Endura does not de-warp the video. You need to load and run a secondary program to dewarp.

- Was able, not with Endura, to dewarp live (Multiple views of same 360 view) both live and recorded.

I understand it works better with some of the other platforms, but Endura is not one. I still have a few up due to location, it is still good to have 360' view.