Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
It's your place to connect with experts and peers, get continuous support, and share knowledge.
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2013-05-22 03:12 AM . Last Modified: 2021-11-08 12:53 AM
Hi.
We faced such a problem. Our customer wants to use Continious recording in Endura system for first 7 days, but Alarm Records should be kept for 30 days for the same cameras.
The question is how to realize this. We cannot delete just continious records avter 7 days. And we cannot record Continious schedule and Alarm Schedule in different pools.
What is you suggestion?
Posted: 2013-05-22 05:58 AM
Hi Sergij,
Please, see the release notes of NSM5200 version 2.2.0.0856:
See point 2 and 3. For position 3 is said that the redundant recording allows you to record cameras on two different pools, which means that you can use different schedules on each pool (this is a native Endura functionality). It is using multicast streams. Find attached the release notes for version 2.3.1.0259. It is written there that the redundant recording allows you to use different schedules on each pool. Use the latest NSM firmware version!
Best regards,
Posted: 2013-05-22 04:08 AM
Hi Sergij,
They should use two storage pools with different recording schedules:
In addition - multicast recording should be used.
Posted: 2013-05-22 04:14 AM
Hi, Plamen. We haven`t used Multicast recording yet. I thought about that solution.
If we use unicast recording and asign cameras to one pool, we cannot asign cameras to another pool.
I hope in case of multicast recording we will be able to asign cameras to two different pools.
Posted: 2013-05-22 04:19 AM
Hi Sergij,
The latest firmware of the NSM allows you to do redundant recording (recording the same cameras on different pools). It has to be checked if unicast or unicast - but we support now redundant recording. I will try to find some info on this.
Posted: 2013-05-22 04:35 AM
Does redundant recording allow to use different schedules for different pools? i doubt about that.
Posted: 2013-05-22 04:38 AM
I will check.
Posted: 2013-05-22 05:58 AM
Hi Sergij,
Please, see the release notes of NSM5200 version 2.2.0.0856:
See point 2 and 3. For position 3 is said that the redundant recording allows you to record cameras on two different pools, which means that you can use different schedules on each pool (this is a native Endura functionality). It is using multicast streams. Find attached the release notes for version 2.3.1.0259. It is written there that the redundant recording allows you to use different schedules on each pool. Use the latest NSM firmware version!
Best regards,
Posted: 2013-05-22 09:38 AM
Please note, the NSM5200 software referenced is Version 2.3.1.0259. This is the latest release as of May, 2013.
Posted: 2013-05-22 11:18 PM
I have a great idea to solve our problem, but it needs some improvements in Endura System.
Endura Settings have such parameters. Delete Scheduled Video in _____days and Delete blocked video in ____ days.
So if Endura system obtains a setting which can allow automatically block alarm video, we will be able to solve the problem.
We will be able to create two schedules for one pool, one for Continious recording and one for Alarms Recording. Continious records will be deleted in 7 days but automatically blocked alarms will be deleted in 30 days.
So we do not need Redundant pools.
Endura already has the possibility to block video manually but it cannot block video automatically. So the question is whether it`s possible to add such feature.
Posted: 2013-05-24 02:45 AM
Hi Sergij,
The automatic video lock (blocking) could be achieved also using the Pelco SDK.
Best regards,
User | Count |
---|---|
67 | |
51 | |
45 | |
16 | |
15 | |
15 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.