Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84306members
353462posts

Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

Archives: Building Automation and Control

Jeff
Administrator Administrator
Administrator

Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

Please find the session 1 recording of our Success with SmartStruxure series attached.  Unfortunately, I missed the first few minutes of the call in the recording, but if there is sufficient interest, we can re-record this portion of the process.

 

The video shows Michael Botens editing the master graphic, placing buttons for each VAV box (that own the bindings for each box), performing bindings, demonstrating functionality, and answering a number of questions from the session chat and from people on the call.

 

This file is a .webm recording.  If you need a video player to handle this file type, I suggest downloading VLC.

 

Thanks to everyone that participated in the call.

 

--Jeff

 

Attachments
10 Replies 10
jingli_an_conve
Lieutenant | EcoXpert Master Lieutenant | EcoXpert Master
Lieutenant | EcoXpert Master

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

Please re-record. Thanks!!

omar_yakobi_con
Ensign
Ensign

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

Re-record please. Cheers!

Vassil
Picard | EcoXpert Master Picard | EcoXpert Master
Picard | EcoXpert Master

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

Yes, please re-record and have the video full length. Thanks.

CraigEl
Administrator Administrator
Administrator

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

+1 for re-recording

LeeCravens
Commander Commander
Commander

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

Also would like to see this re-recorded...sorry guys!

Cody_Failinger
Administrator Administrator
Administrator
0 Likes
0
175

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

I say re-record as well.

JohnBoehmer
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
175

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

Add my vote to the bucket. 

sesa284512
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
175

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

Would love to see the beginning of the recording.  Thanks!

sesa145087_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
175

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

I'd like to see it. But always failed.

Chris_154851
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
175

Re: Success With SmartStruxure - Session 1 - VAV Master Graphics (2014-02-05) Recording

Definitely would like to see the beginning.