Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84589members
353854posts

StruxureWare 1.3 SP1 release

Archives: Building Automation and Control

Derrick_Ratliff
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
2
25

StruxureWare 1.3 SP1 release

You may have noticed that the SP1 for 1.3 is now release on extranet.  Since it is a service pack it requires the 1.3.0 release build to be installed first. The installer will run on top of that build.

If someone hears that this service pack will be required to go to 1.4 post it on this community.

2 Replies 2
SESA116857
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
10

Re: StruxureWare 1.3 SP1 release

It surprises me that it does an uninstall even when you select the upgrade option for Workstation.

It is unclear if you have to be running Workstation 1.3 SP1 or not to work with ES SP1. I suspect it is, but not 100% confirmed in the release notices that I can see.

Derrick_Ratliff
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
10

Re: StruxureWare 1.3 SP1 release

I went ahead and wrote LL#12906 to document this for anyone who skips the release notice.