Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354357posts

SmartStruxure Software Permissions

Archives: Building Automation and Control

PatM
Lieutenant Lieutenant
Lieutenant

SmartStruxure Software Permissions

This video will show you how to add software permissions to SBO users and user groups using three different methods:

  1. Manually add Path Permissions in the Software Permissions tab of a User or User Group
  2. Drag and drop folders and containers from the System Tree into the Path box in the Software Permissions tab of a User or User Group
  3. Right-click on a folder or container in the System Tree and pick Edit Permissions

Video Link : 2550

Attachments
1 Reply 1
Benji
Administrator Administrator
Administrator

Re: SmartStruxure Software Permissions

Any reason this is not in the main SmartStruxure sub Community rather than Area360 which is US oriented? Seems it could have value for many people.