Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84721members
354122posts

SmartStruxure-Alarms-Using Alarm state

Archives: Building Automation and Control

Bob_Schultz
Schneider Alumni (Retired)
Schneider Alumni (Retired)

SmartStruxure-Alarms-Using Alarm state

 

A SmartStruxure Alarm Object has an integer output called the Alarm state.

     0 = Normal

     1 = In Alarm, not acknowledged

     2 = In Alarm, acknowledged

     3 = Aalrm Condition Returned to Normal, but the alarm was never acknowledged.

 

In this video we will walk through a case study that uses this alarm output as part of control logic.

Attachments
2 Replies 2
David_Purser
Spock Spock
Spock

Re: SmartStruxure-Alarms-Using Alarm state

4 = Disable

I configure my alarms with FanCmd is monitored variable and FanSts is shunt variable. So when shunted (Cmd=On and Sts=On), the alarm is Disabled. I consider Disable to be a NORMAL condition.

Also Disable is the state of the alarm if no monitored variable is bound.

Reminder: use the Integer Input to bind to the AlarmState from the alarm object directly or multistate value. It is in the video, of course, but since I rarely use it I forgot and used an Real Input, which does not bind.

David_Purser
Spock Spock
Spock
0 Likes
0
60

Re: SmartStruxure-Alarms-Using Alarm state

https://exchangecommunity.schneider-electric.com/docs/DOC-7957

 

Here is an example of Display bubble configured to bind to AlarmState and show Text - Normal, Alarm, Fault and indicate Alarm for alarm conditions.