Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84294members
353432posts

SE Americas SmartStruxure Demo Database

Archives: Building Automation and Control

Mike
Janeway Janeway
Janeway

SE Americas SmartStruxure Demo Database

This is the Schneider Electric Americas Struxureware Building Operation demo database.

Attachments
5 Replies 5
Rajakumar_K
Lt. Commander
Lt. Commander
0 Likes
0
262

Re: SE Americas SmartStruxure Demo Database

Hi Michael Botens,

I tried to import DEMO DB in SBO 1.9.1 version, but its failed to import.

So could you share the DB in xbk or tgml format.

Benji
Administrator Administrator
Administrator
0 Likes
1
262

Re: SE Americas SmartStruxure Demo Database

Don’t know if it’s the same you have here?

https://schneider-electric.box.com/s/02q105em4d7ymtihytdlv65vzm8bvh2w

Rajakumar_K
Lt. Commander
Lt. Commander
0 Likes
0
262

Re: SE Americas SmartStruxure Demo Database

xbk file is OK.

Alan_McComas
Captain | EcoXpert Master Captain | EcoXpert Master
Captain | EcoXpert Master
0 Likes
0
259

Re: SE Americas SmartStruxure Demo Database

Does anyone know if there are component libraries available for AHU-1 and AHU-3 in the EBO 2.0 Demo? -Alan
dvir
Commander Commander
Commander
0 Likes
0
174

Re: SE Americas SmartStruxure Demo Database

 

Hi when I try to insert this file, it alerts me about a size problem

Do you know of another way to insert the file?

Thanks

 

 

Attachments