Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84521members
353752posts

How to trace AS or ES send an email to SMTP server

Archives: Building Automation and Control

YangboLIU
Commander Commander
Commander
0 Likes
3
55

How to trace AS or ES send an email to SMTP server

I want to send an email when alarm happens but failed, I don't know where I make a mistake. The alarm works but no email send out, both failed with Schneider email server and Netease email server.

I use eventview to view the events, but there is no information about email notification in the alarm events, Anyone can tell me how to know the alarm triggered the email notification or not.

Thanks and Regards

Yangbo

3 Replies 3
SangKim
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
2
22

Re: How to trace AS or ES send an email to SMTP server

Hi Yangbo,   Please check the LL#16250 submitted by Benji.

For wireshark capturing filter, you can also use "tcp port 25 and host 10.20.30.40 and len > 100".

* The IP address 10.20.30.40 is the IP of the device that sends out the SMTP email.

YangboLIU
Commander Commander
Commander
0 Likes
1
22

Re: How to trace AS or ES send an email to SMTP server

HI Sang

Thank you for help. Got it.

Regards

Yangbo

Julio_Cortes
Commander Commander
Commander
0 Likes
0
22

Re: How to trace AS or ES send an email to SMTP server

the SMTP filter should work and I would also look for the built in filters under the expressions.