Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84475members
353691posts

EchoLake

Archives: Building Automation and Control

Nava
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
2
80

EchoLake

With the advent of smart spaces, it is becoming more and more desirable to have a more natural user interface for interacting with one's environment, and what is more natural than speech? If we could somehow find a way to use speech in control our SBO system, that could really give us an advantage in the healthcare and hotel markets. Introducing EchoLake!

EchoLake enables SBO to be controlled using the Amazon Echo via Amazon Alexa and features the ability to:

  • Read property values from SBO while talking to the Amazon Echo
  • Set property values in SBO while talking to the Amazon Echo

License:

NOTE: This is only a proof of concept, and has not been 'hardened' for commercial use.


Developer: not provided

Current Version: not provided

Support Contact: not provided

* Zip files and User Guide are attached.


Please rate this extension!

Attachments
2 Replies 2
Vassil
Picard | EcoXpert Master Picard | EcoXpert Master
Picard | EcoXpert Master
0 Likes
0
74

Re: EchoLake

Hi Nava, 

 

How do we get the files, user guide, and the license?

The link to SmartConnector Server above is not workig, but in any rate, I don't see a license either on

https://www.smartconnectorserver.com/marketplace

 

JeffBowman
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
58

Re: EchoLake

Hi Vassil,

 

This Extension was used for testing the marketplace in the old exchange and should have never been made public. During the migration the permissions on this were incorrectly set.

 

Sorry for the confusion! There are no files or documentation for you :(.

 

That said, keep checking back as there might be some good stuff coming on the near future with regards to this type of functionality.

 

Regards,

 

-Jeff