Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84375members
353556posts

Critical bug in 1.1.5

Archives: Building Automation and Control

Benji
Administrator Administrator
Administrator
0 Likes
3
82

Critical bug in 1.1.5

There have been a change in TAC Graphics Editor 1.1.5.
 
If you have a component in your component library that has a name with space in it (eg. "Optical Detector"), the editor will crash when you try to save the graphic, or you try to edit the name of the component, after you drag the component onto the drawing.
 
I consider this critical. No warning no nothing. Just a crash of the editor.
3 Replies 3
Vassil
Picard | EcoXpert Master Picard | EcoXpert Master
Picard | EcoXpert Master
0 Likes
2
47

Re: Critical bug in 1.1.5

Also, if your component name starts with a digit such as 3Way or 3-Way_Valve; Not sure if a dash (-) in the name is a good idea either. It is better to be safe.

Benji
Administrator Administrator
Administrator
0 Likes
1
47

Re: Critical bug in 1.1.5

Thanks for the update. I'll forward it.

/Benji

DavidFisher
Administrator Administrator
Administrator
0 Likes
0
47

Re: Critical bug in 1.1.5

Both of these conditions have been entered as defects.