Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84832members
354293posts

AET: How to install and register the Automated Engineering Tool

Archives: Building Automation and Control

Justin_Javier
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
3
550

AET: How to install and register the Automated Engineering Tool

AET Quick Help Video

Topic: How to install or upgrade AET

 

 

Installing AET is a very easy process.  The setup file can be used to do a brand new install or an upgrade.  In an upgrade, the installation process will uninstall any previous version and will upgrade you to revision on the setup file.  If this is a fresh install, you can follow these basic steps.

 

Installation Basic Steps:

  • Double-click on setup file
  • Accept the License Agreement
  • Click Install
  • Click Finish (Software is now installed on machine)

 

Registration Basic Steps:

  • Open AET from the Start menu
  • Run AET
  • Complete registration form and click Register (You are now registered)

 

 

 

If you have any questions or concerns regarding this topic, please leave a comment below.  For troubleshooting issues, email: Support360@se-360.com and add AET to the front of the subject line and we will get back to you as soon as possible.

3 Replies 3
RonPeters_MBI
Lt. Commander
Lt. Commander
0 Likes
0
224

Re: AET: How to install and register the Automated Engineering Tool

Good Morning,

I watched the Webinar presentation on AET 101 yesterday and I downloaded version 1.9, but it is not recognizing that I had registered v1.8.5.4 and is asking for email and password or a security code to re-register.  Also, the two other links mentioned in the powerpoint are not working for PCT and the Templates.  Please help.

Thank You and May GOD Bless,

Ron

rpeters@masonbarry.com

Trautman_Tom
Lieutenant | EcoXpert Master Lieutenant | EcoXpert Master
Lieutenant | EcoXpert Master

Re: AET: How to install and register the Automated Engineering Tool

I had the same issue. 

Rename the AETLicense.lic file to AETLicenseOld.lic

The file is located here C:\ProgramData\Schneider Electric\AET\License File

  Once you have done this, restart AET.

Engineering Manager FA
The K Company
RonPeters_MBI
Lt. Commander
Lt. Commander
0 Likes
0
224

Re: AET: How to install and register the Automated Engineering Tool

It saw that I had already installed AET on another PC so I unassigned the license from that pc, but now it won't license this pc.